PolarFire® System-on-Chip (SoC) Applications - Inter-Integrated Circuit (I2C)

Last modified by Microchip on 2026/10/19 16:53

Introduction

The Inter-Integrated Circuit (I2C) protocol is a widely used solution that facilitates communication between multiple devices over a short distance.I2C Bus Logo

This article describes the I²C capabilities of the PolarFire® System-on-Chip (SoC) devices and explains how to use the I²C peripheral on PolarFire SoC boards using:

  • Linux® userspace with the i2c-tools utility and C applications
  • A bare-metal I²C application

Prerequisites

Hardware Setup

  1. This application applies to the following PolarFire SoC–based boards:
  2. Linux host PC for the Yocto Project® building environment or Windows Subsystem for Linux (WSL) on a Windows® machine
  3. THERMO 5 Click board™ (MIKROE-2571) for experiments
  4. Digital logic analyzer (optional, but useful for observing and analyzing signals)

Software Setup

  1. SoftConsole® IDE
  2. Libero® SoC Design Suite 2024.2+
  3. Yocto Project host environment

Additional Resources: I²C Protocol Background

Programming a Reference-Design Into SoC

To use the Microcontroller Subsystem (MSS) I²C peripheral in an application, it must first be enabled in the Libero SoC design suite design file.

This example uses the MSS I2C_0 peripheral connected to the mikroBUS™ socket.

PolarFire SoC Icicle Kit

Program the reference design so the system can be used later with the Yocto Project. To use the I²C peripheral, you must know how it is connected in the design. The following table shows the connections for the PolarFire SoC Discovery Kit and the PolarFire SoC Icicle Kit: 

Icicle Kit Discovery Kit
I2C 0Physical ConnectionI2C 0Physical Connection
SDAMBUS socket SDA pinSDAMBUS socket SDA pin
SCLMBUS socket SCL pinSCLMBUS socket SCL pin

We will rely on the PolarFire SoC Icicle Kit's Libero SoC design suite reference design file.

Start by downloading the Icicle kit reference design generation FlashPro images from the latest release in the PolarFire SoC GitHub® repository:

https://github.com/polarfire-soc/icicle-kit-reference-design/releases

Because the I²C protocol requires both the SCL (clock) and SDA (data) lines to operate as inputs and outputs at different times, a Bidirectional Buffer (BIBUF) must be used in the design.

SCL (clock) and SDA (data) lines

Information

Note: If the reference design is used, no modifications are required because the bidirectional buffers are already implemented.


Program the Field-Programmable Gate Array (FPGA) by the MPFS_ICICLE_KIT_BASE_DESIGN_{VERSION}​​​​ ​​​design using the FlashPro Express tool (included with the Libero SoC design suite software).

Open FlashPro Express and program the FPGA fabric using the prebuilt reference programming files.

Open FlashPro Express.

Create New Project.

Warning

Choose the MPFS_ICICLE_KIT_ES_*\MPFS_ICICLE_KIT_ES_BASE_DESIGN_*\MPFS_ICICLE_KIT_ES_*.job file from the reference design download folder.

Click the Run button.

Warning

You have two choices for programming the FPGA:

  1. Use prebuilt reference programming files only (quick start).
  2. Follow "PolarFire® SoC Applications - MSS and Libero® SoC Design Suite" to build/modify the  Libero SoC Design Suite design file and regenerate the programming file.

Now you have programmed the FPGA Fabric logic.

Back to Top

I²C in Linux® Environment

We need to set up and configure the MSS I2C peripheral in the Linux configuration, which is why we need a Linux build system to configure it. For this article, we will use the Yocto Project.

HSS Configurations

Hart Software Services (HSS) is the bootloader used on PolarFire SoC devices. It runs first, sets up hardware, and launches Linux or other apps—essential for multi-core and secure boot.

Objectives:

  • Download and import HSS to SoftConsole.
  • Update references and build HSS.
  • Deploy HSS to PolarFire SoC Icicle Kit.
Information

This application article is verified on HSS 2025.07.

First, download HSS from the hart-software-services GitHub repository.


Import the HSS project to SoftConsole by selecting File > Import > Import Existing Project Into Workspace.

Import window

Browse the HSS folder and import the project into the workspace by clicking Finish.

Warning

Ensure that you checked Copy projects into workspace.


Copy your MSS XML file into the project.

Copy the XML file to hart-software-services/boards/mpfs-icicle-kit/soc_fpga_design/xml/<your xml>.xml.

Information

Note: If your board is a production board (not ES), use boards/mpfs-icicle-kit/... instead of boards/mpfs-icicle-kit-es/...


Copy and rename configurations for HSS.

  1. Copy hart-software-services/boards/mpfs-icicle-kit/def_config to ​​​​​​hart-software-services/
  2. Rename def_config to .config
  3. Edit .config file and update path to your xml by changing next line
CONFIG_SOC_FPGA_DESIGN_XML="boards/mpfs-icicle-kit/soc_fpga_design/xml/<your xml>.xml"

Build HSS and deploy.

Right click on the project name. 

Click on the build project. 

Select the PolarFire SoC program non-secure boot mode 1 run option and deploy the project to SoC. 

Warning

Ensure your run configurations are set correctly. If not, open External tools > External tools configurations and update the die and package with your board parameters. The die for the Icicle Kit ES is MPFS250T_ES and the package is FCVG484.

Back to Top

Yocto Project® Configurations

In this section, we will create a Linux image and program it into the PolarFire SoC Icicle Kit.

Objectives:

  1. Setting up the Yocto Project Building Environment
  2. Enabling the I2C peripheral and including the necessary packages in the build
  3. Building a Linux image and deploying it into the SoC

Creating Environment

To create the Linux build environment, refer to the "OpenEmbedded/Yocto Project BSP layer for Microchip's SoCs" guide on GitHub.


Configuring I²C Peripheral

Prepare the Microchip Linux kernel (linux-mchp) source tree for local development.

MACHINE=mpfs-icicle-kit devtool modify linux-mchp
Success

We should get the following log:

Recipe linux-mchp now set up to build from /build/workspace/sources/linux-mchp


Add the required libraries and applications to the build. Open the conf/local.conf file and add the following variable at the end of the file.

CORE_IMAGE_EXTRA_INSTALL += "i2c-tools packagegroup-core-buildessential vim"

Information
  • i2c-tools - is a Linux package with command-line utilities to scan, read, write, and debug I²C devices. Key commands:
    • Tools:
      • i2cdetect: scan for devices
      • i2cget: read register
      • i2cset: write register
      • i2cdump: dump all registers
    • Perfect for quick I²C testing from userspace.

  • packagegroup-core-buildessential - A Yocto Project meta-package that pulls in all the essential build tools needed for compiling software on your embedded system.

    • Includes:

      • gcc → C compiler

      • make → build automation

      • binutils → linker, assembler, etc.

      • pkgconfig → helps locate libraries and headers

      • libc-dev → standard C library headers

      • autoconf, automake, libtool → for building autotools-based projects

  • vim - A powerful text editor used in terminal environments

Save the file and exit.


Open the Linux Kernel configuration menu to enable the I2C peripheral.

MACHINE=mpfs-icicle-kit bitbake linux-mchp -c menuconfig


Navigate down to the Device Drivers.

Kernel Configuration window


Enable the I2C Support option.

Device Drivers window


Save the config by selecting Save > Exit.


Locate the Icicle kit-related Device Tree Source (DTS) files for modification:

yocto-dev/build/workspace/sources/linux-mchp/arch/riscv/boot/dts/microchip/mpfs-icicle-kit.dts
yocto-dev/build/workspace/sources/linux-mchp/arch/riscv/boot/dts/microchip/mpfs-icicle-kit-common.dtsi

Make sure that the I2C0 peripheral is enabled in the mpfs-icicle-kit-common.dtsi:

1
2
3
&i2c0 {
 status = "okay";
};

Compile a customized Yocto Project Linux kernel recipe in a developer-friendly way, producing kernel binaries for PF SoC:

MACHINE=mpfs-icicle-kit devtool build linux-mchp
Warning

You can create a bbappend layer execute following commands`
> devtool finish linux-mchp custom-layer

​​​​Your bbappend layer will be saved at: custom-layer/recipes-kernel/linux/linux-mchp_%.bbappend

Building Linux Image and Deploying

Execute the following command to build the Linux image:

MACHINE=mpfs-icicle-kit bitbake mchp-base-image

Information

Note: Ensure that the initial Linux image has been built without error, so we can start making the modifications.

Here's the list of names of supporting machines:

MACHINEBoard NameDescription
MACHINE=mpfs-icicle-kitMPFS-ICICLE-KIT-ES, MPFS-ICICLE-KITPolarFire SoC Icicle Kit
MACHINE=mpfs-disco-kitMPFS-DISCO-KITPolarFire SoC Discovery Kit
MACHINE=mpfs-video-kitMPFS250-VIDEO-KITPolarFire SoC Video Kit

After the build completes, the Linux image can be found at:

yocto-dev/build/tmp-glibc/deploy/images/<board_name>/<image-name>.rootfs-***.wic


Follow the GitHub "Programming a Linux Image" instructions to deploy the built Image to the eMMC/SD card memory.

Information

Note: For additional information, refer to the "OpenEmbedded/Yocto Project BSP layer for Microchip's SoCs" page on GitHub.


After booting Linux on the PolarFire SoC Icicle Kit, log in as root and check if the I2C device 0 appears under the devices:

root@icicle-kit-es:/# ls /dev | grep i2c
i2c-0
i2c-1
i2c-2

If no devices are listed, the I²C device may not be enabled. You have to double-check the configuration and DTS modifications that need to be done.

Software Tools and Utilities

i2c-tools Utility

i2c-tools is a utility program used to test and verify the functionality of I2C devices on Linux systems. It is typically used to send and receive data over I2C to ensure that the I2C bus and connected devices are working correctly.

The i2c-tools program interacts with the I2C device driver through the /dev/i2c-X device files, where X represents the bus number. It allows users to perform basic read and write operations, configure I2C settings, and observe the data exchanged between the host (master) and the I2C target device (slave).

Tools of i2c-tools

The i2c-tools package provides utilities for accessing the I²C driver from Userspace.

The following commands are included in i2c-tools:

  • i2cdetect: List all I2C buses present on the system and scan for devices on a specified bus.
  • i2cdump: Display the contents of an I2C device's registers.
  • i2cget: Read values from specified registers of an I2C device.
  • i2cset: Write values to specified registers of an I2C device.
  • i2ctransfer: Perform complex I2C transactions, including multiple read and write operations in a single command.
Using i2c-tools on Icicle kit
Information

Note: All the following commands are running from the Icicle kit connected with the THERMO 5 Click board on the mikroBUS socket.

Icicle with Thermo 5

i2cdetect: Scan for I2C devices connected to the bus. In our case, the THERMO 5 Click board is connected on Bus 0 with a target address of 0x4c:


root@mpfs-icicle-kit:~# i2cdetect -y -r 0
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:                         -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- 4c -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

-y: This option is to run without asking for confirmation.

-r: This option performs a more detailed read-based scan.

i2cdump: Display the contents of a MIKROE-2571's registers:

root@mpfs-icicle-kit:~# i2cdump -y 0 0x4c
No size specified (using byte-data access)
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
00: 22 00 04 80 06 55 00 55 00 80 06 55 00 55 00 00    ".???U.U.??U.U..
10: 00 00 00 00 00 55 00 00 00 55 55 0e 00 00 00 00    .....U...UU?....
20: 55 0a 70 00 00 0e 07 12 12 20 00 00 55 00 00 00    U?p..???? ..U...
30: 55 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00    U?..............
40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
60: 06 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ?...............
70: 06 06 06 00 00 00 00 00 00 00 00 00 00 00 00 00    ???.............
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 28 d4 44 6f    ............(?Do
b0: 20 20 00 00 00 00 00 00 00 00 00 00 00 00 00 00      ..............
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 25 5d 04    .............%]?
Success

We can see the Manufacturer ID with Register Address 0xfe = 5d & Revision ID with Register Address 0xff = 04.

i2cget: Read values from specified registers of the MIKROE-2571 device. To read Product ID from register address 0xFD:

# i2cget -y 0 0x4c 0xfd
0x25

I2C EMC logic

i2cset: Write values to specified registers of the MIKROE-2571 device. To write value 0x24 to Internal Diode Therm Limit (0x20):

i2cset <bus> <Target_Address> <Register_address_to_be_written> <the_value_to_be_write>

# i2cset -y 0 0x4c 0x20 0x24

i2ctransfer: Perform complex I2C transactions like performing a combined write and read operation. To read one byte from address 0xfe:

# i2ctransfer -f -y 0 w1@0x4c 0xfe r1@0x4c
0x5d
  • 0: This represents the I2C bus number.
  • w1@0x4c 0xfe: Write 1 byte (0xfe) to the device at address 0x4C to set the register pointer.
  • r1@0x4c: Read one byte from the device at address 0x4C.

Application Programming in C Language Using i2c-dev

We can write a C program that runs from Userspace and interacts with I2C devices using the ioctl functions. The following example C program reads the internal diode temperature registers, converts the values to degrees Celsius, and prints the results.

Boot Linux on your Icicle kit. Navigate to /media and create i2c_mikroe2571.c using the vim editor.

cd /media && vim i2c_mikroe2571.c

Copy and paste the following C code to i2c_mikroe2571.c:

#include <stdio.h>
#include
<stdlib.h>
#include
<stdint.h>
#include
<unistd.h>
#include
<fcntl.h>
#include
<sys/ioctl.h>
#include
<linux/i2c.h>
#include
<linux/i2c-dev.h>
#include
<errno.h>

#define I2C_BUS "/dev/i2c-0"
#define MIKROE2571_ADDR 0x4c

// Example MIKROE-2571 register addresses (update as needed)
#define INTERNAL_DIODE_HIGH 0x00
#define INTERNAL_DIODE_LOW  0x29
#define EXT1_DIODE_HIGH     0x01
#define EXT1_DIODE_LOW      0x10
#define EXT2_DIODE_HIGH     0x23
#define EXT2_DIODE_LOW      0x24
#define EXT3_DIODE_HIGH     0x2a
#define EXT3_DIODE_LOW      0x2b

// Function to read a single 8-bit register
int read_register8(int file, uint8_t reg, uint8_t *value) {
   if (write(file, &reg, 1) != 1) {
        perror("Failed to write register address");
       return -1;
    }
   if (read(file, value, 1) != 1) {
        perror("Failed to read register value");
       return -1;
    }
   return 0;
}

int main() {
   int file;
   int retries = 5;
   uint8_t temp_int, temp_frac;
   uint8_t ext1_int, ext1_frac;
   uint8_t ext2_int, ext2_frac;
   uint8_t ext3_int, ext3_frac;

   // Open the I2C bus
   if ((file = open(I2C_BUS, O_RDWR)) < 0) {
        perror("Failed to open the I2C bus");
        exit(1);
    }

   // Retry setting the I2C address if the bus is busy
   while (retries--) {
       if (ioctl(file, I2C_SLAVE, MIKROE2571_ADDR) < 0) {
           if (errno == EBUSY) {
                printf("I2C bus is busy, retrying...\n");
                sleep(1);
               continue;
            } else {
                perror("Failed to acquire bus access and/or talk to slave");
                close(file);
                exit(1);
            }
        }
       break;
    }

   if (retries <= 0) {
        printf("Failed to acquire bus access after multiple attempts\n");
        close(file);
        exit(1);
    }

   while (1) {
       // Read internal diode temperature (high and low byte)
       if (read_register8(file, INTERNAL_DIODE_HIGH, &temp_int) < 0 ||
            read_register8(file, INTERNAL_DIODE_LOW, &temp_frac) < 0) {
            close(file);
            exit(1);
        }

       // Read external diode 1
       if (read_register8(file, EXT1_DIODE_HIGH, &ext1_int) < 0 ||
            read_register8(file, EXT1_DIODE_LOW, &ext1_frac) < 0) {
            close(file);
            exit(1);
        }

       // Read external diode 2
       if (read_register8(file, EXT2_DIODE_HIGH, &ext2_int) < 0 ||
            read_register8(file, EXT2_DIODE_LOW, &ext2_frac) < 0) {
            close(file);
            exit(1);
        }

       // Read external diode 3
       if (read_register8(file, EXT3_DIODE_HIGH, &ext3_int) < 0 ||
            read_register8(file, EXT3_DIODE_LOW, &ext3_frac) < 0) {
            close(file);
            exit(1);
        }

       // Print the temperature values (raw, conversion to Celsius as needed)
       printf("Internal: 0x%02X 0x%02X | Ext1: 0x%02X 0x%02X | Ext2: 0x%02X 0x%02X | Ext3: 0x%02X 0x%02X\n",
            temp_int, temp_frac, ext1_int, ext1_frac, ext2_int, ext2_frac, ext3_int, ext3_frac);

        sleep(1);
    }

    close(file);
   return 0;
}

After saving the modification, compile the C code:

gcc -o i2c_mikroe2571 i2c_mikroe2571.c -li2c

Run the i2c_mikroe2571 executable:

./i2c_mikroe2571
Success

Running the application will return the following response:

root@mpfs-icicle-kit:/media# ./i2c_mikroe2571
Internal: 0x1E 0x40 | Ext1: 0x00 0x00 | Ext2: 0x00 0x00 | Ext3: 0x00 0x00
Internal: 0x1E 0x20 | Ext1: 0x00 0x00 | Ext2: 0x00 0x00 | Ext3: 0x00 0x00
Internal: 0x1E 0x40 | Ext1: 0x00 0x00 | Ext2: 0x00 0x00 | Ext3: 0x00 0x00

The values do not represent the actual temperature, as it needs to be converted to Celsius.

Back to Top

I²C in Bare Metal Applications

To use the MSS I²C peripheral in a bare metal application, we have to use the SoftConsole to develop the application to build, compile, and deploy.

This example uses a bare metal reference application from the official GitHub repository and modifies it to use the MSS I2C_0 peripheral to communicate with the MIKROE‑2571 device.

Download the mpfs-blank-baremetal bare metal application project from the mpfs-blank-baremetal repository on GitHub and import it into SoftConsole.

Note: If this is your first time importing a project in SoftConsole, watch this video:

 


Replace the MSS Configuration XML file in the bare metal project with the XML file used in your Libero SoC design suite design file. The path to the file that SoftConsole will use to generate header files, which are then used by the MPFS HAL, is:

mpfs-blank-baremetal > "your_board" > fpga_design > design_description > xx.xml

Now we can begin modifying u54_1.c with our custom code to perform the following:

  • Read the ID of the MIKROE-2571 from register 0xFF, referring to the data sheet.
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
#include <stdio.h>
#include
<string.h>
#include
"mpfs_hal/mss_hal.h"
#include
"drivers/mss/mss_mmuart/mss_uart.h"
#include
"drivers/mss/mss_i2c/mss_i2c.h"


#define MY_ADDR 0x21u
#define SLAVE_ADDR 0x4cu
#define SLAVE_REVISION_ID_REG 0xffu
#define TX_BUF_SIZE  1u

static uint8_t tx_buffer[TX_BUF_SIZE];
static uint8_t rx_buffer[10];

void u54_1(void)
{
    PLIC_init();
    PLIC_SetPriority(I2C0_MAIN_PLIC, 2);
    __enable_irq();

    (void) mss_config_clk_rst(MSS_PERIPH_MMUART1, (uint8_t) 1, PERIPHERAL_ON);
    (void) mss_config_clk_rst(MSS_PERIPH_I2C0   , (uint8_t) 1, PERIPHERAL_ON);


    MSS_I2C_init(&g_mss_i2c0_lo, MY_ADDR, MSS_I2C_PCLK_DIV_192);

    MSS_UART_init(&g_mss_uart1_lo,
        MSS_UART_115200_BAUD,
        MSS_UART_DATA_8_BITS | MSS_UART_NO_PARITY | MSS_UART_ONE_STOP_BIT);

    MSS_UART_polled_tx_string(&g_mss_uart1_lo, "\r\nChecking connection to MIKROE-2571\r\n");

    tx_buffer[0] = SLAVE_REVISION_ID_REG;
    MSS_I2C_write_read(
               &g_mss_i2c0_lo,
                SLAVE_ADDR,
                tx_buffer,
                TX_BUF_SIZE,
                rx_buffer,
               1,
                MSS_I2C_RELEASE_BUS
            );

    (void)MSS_I2C_wait_complete(&g_mss_i2c0_lo, 3000u);

   if(rx_buffer[0] == 0x04u){
        MSS_UART_polled_tx_string(&g_mss_uart1_lo, "Connected Successfully");
    } else {
       uint8_t message[40] = {};
        sprintf((char*)&message, "\r\nUnable to connect!\r\nReceived: 0x%X \r\n", (uint8_t)(rx_buffer[0]));
        MSS_UART_polled_tx(&g_mss_uart1_lo, message, 40);
    }

}

Line 1-14: We start by including the necessary header files for standard input/output, string handling, and the PolarFire SoC HAL, UART, and I2C drivers. We also declare global variables for UART and I2C communication.

Line 16-23: The u54_1() function is the main entry point for the application. It waits for a software interrupt to synchronize startup and enables the required peripherals.

Line 26-32: We initialize the UART and I2C peripherals, I2c as a host.

Line 34-45: Trying to read  MIKROE-2571 Revision ID number (0x4h) and store in rx_buffer.

Line 47-53: Checking for wrong data, if data is right, transmitting complete message via UART, else transmitting Fail message.


Build the project and deploy it either in LIM for Debug mode or eNVM for Release mode.

Note: You can watch the "Build and Debug the Project" video for bare metal applications in SoftConsole.

Back to Top

Summary

This article explains how to enable and test I²C communication on PolarFire SoC boards using the Yocto Project. The process begins with configuring the device tree to enable the I2C peripheral, then ensuring the I2C driver is enabled in the Linux kernel. Userspace testing can then be performed using the i2c-tools utility to interact with I2C devices from the Linux Userspace. Additionally, a custom C program is written and executed to read temperature register values/device ID from an I2C device. By following this guide, you establish a solid foundation for further development with I2C peripherals on the PolarFire SoC-based boards.

Back to Top