Getting Started with MCU Projects Using MPLAB® Code Configurator (MCC) Melody
Editing an Existing MPLAB® Code Configurator (MCC) Melody Project
| Building an MCC Melody Project and Programing a Development Board | Debugging an MCC Melody Project with the Data Visualizer |
MCC Melody Tour
In this section, the MPLAB® Code Configurator (MCC) Melody plug-in will be opened, its key features will be highlighted, and the various configurations used to set up the project will be examined.
This class was developed using the latest version of the MPLAB X IDE (v6.20) and MCC Melody plug-in (v5.5.0) at the time. These tools are always evolving with updates being made. Our recommendation would always be to try and use the latest version of the toolchain when developing applications, especially with newer devices.
Let’s now open MCC Melody and take a tour. To access MCC Melody, click on the blue shield icon
at the top of MPLAB X IDE.
If the downloaded project was created with an older version of the tools, you might be prompted to upgrade to a more recent version of the toolchain. This is advisable as updates often address known issues in previous versions. However, if necessary, you can always revert to an older version using a feature known as the content manager.
Depending on the version of the toolchain you're using, you may need to choose between MCC Classic and MCC Melody. Choose MCC Classic only if the project you're evaluating was developed using MCC Classic or if your device isn't compatible with MCC Melody. For all newer devices and projects, MCC Melody is the recommended choice, as all future support and development will be focused on it. You may also be given the option to load various libraries, but this won't be utilized in this demonstration. However, if necessary, you can add libraries later using the content manager.
Let’s take a moment to go through the essential features of the tool.

Project Resources
In the standard Window configuration, you will notice the Project Resources section situated at the top left of the tool. This section shows the integrated peripherals, external components, and libraries the MCC Melody project is using. You will also find components in the System Modules, which are included by default in any project and cannot be removed. These modules are named Clock Control, Configuration Bits, Interrupt Manager, Main, and Pins.
Clock Control
Configuration Bits
Interrupt Manager
Main
Pins
Device Resources
Pin Package and Pin Grid Views
Next to the Pin Package view, you'll see the Pin Grid View. This view displays all available pins for your chosen microcontroller in a grid format. Package pin numbers are positioned at the top of the grid, with most pins having an associated PORT and individual port bit number listed directly underneath. Each grid row signifies an available device resource signal, and by clicking the corresponding cell, you can assign the signal to a pin.
Many devices allow various signals on the device to be routed to different pins and can even be rerouted at run time dynamically. Signals that have been assigned are highlighted in green with a lock icon on the relevant pins. Available pins are either blue with an unlocked icon, indicating that the associated signal can be used on multiple pins, or orange, indicating that the signal can only be used on one pin at a time.
For example, expanding the Peripherals menu on the Microcontroller component reveals System and Peripheral resources available on the device. Expanding the Universal Asynchronous Receiver Transmitter (UART), reveals not only how many instances of the peripheral are available on the device but also how they interface with the other components.
So that was a quick tour of the main components found in MCC Melody.
Working with Device Resources
In this section, you'll see how you can configure a selected target Microcontroller by editing the project downloaded from the Discover tool earlier in the class.
Drivers are employed when you, as a developer, want to configure peripherals or features using a graphical representation of the resource.
Inside of the builder window you’ll notice that the UART consists of two peripheral-related components: the driver you just looked at and a second component called the Peripheral Library (PLIB).
PLIBs represent the firmware that will be generated based on your configuration setup in MCC Melody. In some instances, like this one for the UART, an associated Driver will be included. This library indicates that development has been done for this common peripheral that is available on most Microcontroller devices, such as a UART or Timer, to provide an abstraction layer to the associated firmware created, making it more portable if the generated code needs to be ported to a different device.
You can access Device Library-specific resources by hovering over the Driver component in the Builder Window and then clicking the question mark that appears or by clicking the question mark next to a Driver listing inside of the Project Resources window. This will open an associated API reference landing page that explains how to use the various functions, macros, and other firmware components that will be created when the code is generated.
If the resource is a Library, the API reference page will also include use cases, complete with code examples and video overviews.
In the Device Resources section, you’ll also notice a section for Hardware Peripherals. This could be confusing as the Device and PLIB Drivers you just looked at are used to initialize and configure peripherals. Hardware Peripheral initializers are a different way to represent the device resource as associated registers that align with what you would see in the datasheet registers section as opposed to the Easy View used with Drivers.
The choice between which of the two device resource representations you will use depends on your preference and comfort level as a developer.
You can remove the ADC Initializer device resource by clicking on the red X next to the component in the Project Resources listing as it won’t be used in this class.
That’s a high-level overview of how to work with Device Resources. Let’s now look at how we can use what we’ve learned here to modify the Discover Demo Project.
Configuring an MCU and Editing a Project
MCU Clock Configuration
Any changes you make to each Easy View parameter will determine the firmware API that is produced when you click the Generate button. For further details, you can click the question mark next to each parameter, which will direct you to the relevant section of the corresponding datasheet in the online documentation.
For instance, if you reduce the System Clock to 250KHz and open the UART2 Driver Easy View, you will see a high baud rate error percentage for the chosen baud rate.

Additionally, MCC Melody features a Notifications tab at the bottom of the tool window. When you click this tab, it displays any relevant Errors, Warnings, or Hints, including a note in this scenario that the Baud Rate error surpasses the recommended 2 percent.
When you develop applications at the register level, you might unintentionally encounter issues beyond mere syntax errors. Take the UART baud rate example provided, for instance. Despite the baud rate error exceeding 2 percent, the corresponding code would have compiled successfully. Yet, communication via the UART would be inconsistent, which could result in much time bench testing to locate the problem's source. By employing MCC Melody, you could identify the problem early in the development phase and mitigate costly debugging and redesign.
Let’s look at how this will affect our application by generating the code (click Generate
) and then downloading it to the Curiosity Nano board (click Make and Program Device
).
Evaluating the output in the Data Visualizer Terminal and pressing the pushbutton on the Curiosity Nano board, you would expect an upper case ‘S’ but instead you get some random character. Entering an upper case ‘T’ in the terminal you would expect the LED on the Curiosity Nano board to toggle ON/OFF but nothing happens.
Of course, you know why the application isn’t working. Let’s go ahead and fix the application inside of MCC Melody.
UART Driver Configuration
As mentioned earlier, some standard peripherals like the UART have their related peripheral libraries abstracted to improve portability across devices. In these cases, the PLIB Easy View needs to identify the peripheral or feature on the target device that should be assigned to it, or in other words, determine the PLIB's dependency. When you scroll down through the PLIB Easy View to the Dependency Selection, you select the UART dependency from the UART Dependency Selection dropdown.
Clicking on the UART2 driver block opens the UART2 Easy View, which was previously used to verify the baud rate error percentage.
In the UART Driver Easy View, in the Configuration Settings area, the baud rate is set to 9600 by manually entering the value into the corresponding Requested Baudrate field. You may notice this is referred to as Requested Baudrate since the actual baud rate will be limited by the previously defined clock configuration.
It is important to note that the Calculated Baudrate, which displays the actual Baud rate based on the clock settings, is located immediately below the Requested Baudrate field. The previously discussed Baud Rate Error is right below the Calculated Baudrate field.
You can find additional UART settings below these fields but those are left at their default settings in this application.
UART and LED Pin Assignment
In this application, the UART sends and receives messages via a serial terminal on your host computer through the USB port. The Curiosity Nano boards come equipped with a UART-to-USB converter built into their debugging circuitry. To establish this connection, you must specifically assign the target microcontroller UART pins to connect to the corresponding circuitry on the Curiosity Nano board.
Referring to the Pin Grid View in the Melody tool, notice that the UART2 peripheral is set to receive RX signals on pin 17, which is PORTB bit 5, and transmit TX data on pin 16 or PORTB bit 4.

The Serial/CDC Port refers to the UART-to-USB converter, and the pins selected in Melody are confirmed as correct, with the UART2 TX signal on RB4 or PORTB bit 4 and UART2 RX connected to RB5. Also note that LED0 connects to pin RC7 and the pushbutton or switch to RA0, as confirmed in the MCC Melody Pin Grid View in the Pins General Purpose Input/Output (GPIO) signal assignment.
The LED connected to RC7 is set as an output, and the switch connected to RA0 is set as an input.

Referring to the open schematics, the first page indicates that both the switch and LED are Active Low.

On the next page of the schematics, at the bottom, you will see that the Anode of the LED connects to a voltage source and the Cathode through a current limiting resistor to pin RC7.
Therefore, driving the RC7 LOW or to 0V will turn the LED ON. The switch connects to the RA0 pin through a current limiting resistor, with the other lead connected to ground. When you press the pushbutton, the connection will complete, and RA0 will be pulled to 0V.
You may notice a critical component missing common to most switch interfaces when following the connection from the switch current limiting resistor to the pin on the Microcontroller on the schematic. A pull-up resistor is typically used to eliminate unwanted noise on the pin and false triggers.
Back to the MCC Melody tool, click on the Pins component inside of Project Resources to open the associated Easy View.

Inside of the Pins Easy View, all the pins selected from the Pin Grid View are shown, including some additional capabilities. You can also rename that pin to something more intuitive than the default name, and this will be reflected in the generated firmware associated with that pin. Looking at the row associated with RA0 shows that the pin is associated with function GPIO, set as an input, the custom name has been set to SW0 to align with the switch name in the PIC18F56Q71 Cnano schematics and that the Weak Pullup is enabled. Most pins on modern PIC and AVR® microcontrollers feature the ability to assign a weak pull up resistor to its input to further reduce the number of external components needed.
Generate Code
Remember that modifications were made to the Clock Frequency for the device earlier changing the system clock frequency to 500 kHz from 1 MHz. These alterations will not take effect until the Generate button
, located at the top of the Project Resources pane, is pressed to regenerate the code.
Code has now been generated for the project based on the changes made. Next, let’s look at how to use this code in an application.
Navigating and Using Generated Code
We can see what actions the macro is performing by clicking on the macro name here while holding down the CTRL key on my Windows® machine.

Using the same technique to navigate to the UART2_Write() we can see that firmware simply assigns a register called U2TXB, an acronym for the UART 2 Transmit Buffer, with the txData parameter which in this case is ‘S’ character. Loading a value into this register automatically triggers a transmit over the UART TX line.
Returning to the main(), before exiting the if statement a 350 ms delay is implemented to avoid sending multiple ‘S’ characters at the same time. Changing the value of delay parameter will change the output to the terminal window. As an example of reducing the delay parameter to say 100 ms and reprogramming the device, we can see that multiple ‘S’ characters are transmitted as the while(1) loops through the check quicker now that we’ve released the button.
On the other hand, adding another zero to get 1000 ms or 1 second and reprogramming the PIC18F56Q71 we can see that now if we press the button too quickly the loop through to the button check may be going so slowly that it might just miss some of the presses. Let’s return the parameter to 350 ms as this seemed to work pretty well.

Clicking on the delay_ms(1) while holding the CTRL key further reveals the associated define inside of the builtins.h file.
So this is a great way to see how code has been created and used within the API that can be used as a reference when creating your own custom code.
If there is a value in the Receive Buffer…or in other words the UART2_IsRxReady() is TRUE, then an 8-bit variable called rxValue defined just before the while(1) is assigned the value. Again, let’s use CTRL and right-click to navigate to the UART_Read(). This is defined as the UART2_Read function call which we can see returns the contents of the UART2 Receive Buffer or U2RXB. An important point here is that only after calling the UART_Read() here will the UART2_IsRxReady() flag be reset. This occurs once the UART2_Read() value is assigned to the rxValue.
The next line of code uses a final if statement which checks the rxValue variable. If it contains the ‘T’ character, then the LED_Toggle() macro is executed. Using the CTRL left-click we can see that the LED_Toggle() macro performs an exclusive OR on the LATC7 bit in the LATC register which will toggle the value output on the RC7 pin connected to the LED.
Now that we have a better understanding of how to navigate and use the code from the basicUARTcomms example, let's now look at how to keep our tools up to date and how we can revert resources using the Content Manager.
Versioning and the Content Manager
There are a few ways that the tools and resources can be updated or reverted for an MCC Melody project.
You could also use the Content Manager button
in the MPLAB X IDE toolbar at the top of the IDE but you will need to close MCC Melody.
If a driver or library update causes your project to malfunction, you have the option to revert to a previous version of the driver or library to restore the application's functionality. For example, within the Content Manager, expanding the Drivers accordion menu reveals a list of all available peripheral drivers.
Each entry includes a version number and indicates whether the driver is the latest version (highlighted in green) or if an update is available (highlighted in yellow), followed by a driver description.
You can view other available driver versions by expanding the drop-down in the Version column.
To revert, simply select an older driver version and click the Apply button at the top of the Content Manager. The update process may take a few minutes, after which the MCC Melody will restart. There is also a Select Latest Version(s) button that, when selected and the Apply button pressed, will automatically update all updatable content. The successful updates will be confirmed in the Output window.
If these files have been misplaced or overwritten, you can still access the original header files in the GitHub repository for the corresponding example.
To do this, navigate to the specific Discover example page, select the Open with drop-down, and click on GitHub.
So that’s it! You should now understand how to open an existing MCC Melody project, make changes, update the generated API and then navigate the code.