Audio-Tone Generation Using a Lookup Table With MPLAB® Harmony v3: Step 5
Last modified by Microchip on 2023/11/09 09:07
Verify I/O Pins Using the Graphical Pin Manager
Open the Graphical Pin Manager by clicking on the Pin Settings tab and select to order by Ports.
Some of the LED and SWITCH pins have already been defined by the BSP. However, you will need to define some additional pins required by this lab. It is important to name the pins exactly as they are listed in the following table. Many of the drivers are referencing these pins using a specific name. The following table is a list of the pins required by all the labs in this series (in port order).

You can also display the pin configuration by selecting the Pin Diagram tab. This gives a quick view of which pins are being used by the device.