Low-Power Application on SAM D21 Using MPLAB® Harmony v3 Peripheral Libraries: Step 4
Configure Power Manager (PM) Peripheral Library
Under the bottom left Device Resources tab, expand Harmony > Peripherals > PM.
Double-click or drag and drop PM to add the PM peripheral library to the project graph.

Figure 1
Select the PM Peripheral Library in the Project Graph window and configure it as shown in Figure 2.

Figure 2
Configure NVMCTRL Peripheral Library
The Non-volatile Memory Controller (NVMCTRL) is added by default to the project graph. Select the NVMCTRL Peripheral Library and configure it as shown in Figure 3.
- Verify that Wait States is configured as 1 to read the non-volatile memory. When the device is put in performance level 0, the device clock frequency cannot exceed 12 MHz, and one wait state is required.
- Set the Power Reduction Mode During Sleep to WAKEUP INSTANT. This bit configures the NVMCTRL to wake up the Flash memory when the CPU wakes up from Standby mode, which allows it to reduce device wake-up time.
- Disable the Instruction Cache to reduce the device's wake-up time. When the cache is enabled, the device will look for an instruction to fetch upon interrupt in the cache at first. If the instruction is found, the device wakes up quicker, but if not, a cache miss occurs and the wake-up time is longer. This option is good to enable when the instruction to fetch upon an interrupt is always stored in the cache memory, which is not the case here, as we have different interrupt sources.

Figure 3
Configure LED and Wake-up Test Pins
Open the Pin Configuration tab by clicking Tools > Pin Configuration.

Figure 4
Once the Pin Settings window is opened, scroll down to pin numbers PA27 and PB30, and then configure these pins as shown in Figure 5:
- Set the Pin Number #51 as GPIO:
- Pin ID = PA27
- Custom Name = WAKEUP_TEST
- Function = GPIO
- Direction = Out
- Latch = High
- Set the Pin Number #59 as GPIO:
- Pin ID = PB30
- Custom Name = LED0
- Function = GPIO
- Direction = Out
- Latch = High

Figure 5