Arm® TrustZone® Technology Getting Started Application on PIC32CM LS60: Step 2
Configure the Secure Real-Time Clock (RTC) Peripheral Library.
Under the bottom left Device Resources tab, expand Harmony > Peripherals > RTC.
Double-click or drag and drop RTC to add the RTC Peripheral Library (PLIB) to the Project Graph.

Figure 1
In the Clock Easy view, verify the RTC clock is set to run at 1 kHz internal ultra-low-power clock.
When a module is added to the Project Graph, MPLAB® Code Configurator (MCC) automatically enables the clock to the module. The default RTC clock source is an internal 1 kHz ultra-low-power clock (OSCULP1K).

Figure 2
Go back to the Project Graph and configure the RTC PLIB to generate a compare interrupt every 500 milliseconds.

Figure 3
Configure the Secure I²C Peripheral Library and Secure I²C pins.
Under the Device Resources tab, expand Harmony > Peripherals > SERCOM.
Double-click on SERCOM5 to add the SERCOM Instance 5 to the project.

Figure 4
Select the SERCOM 5 Peripheral Library and configure it for the I²C protocol as shown in Figure 5.

Figure 5
Open the Pin Configuration tabs by clicking Project Graph > Plugins > Pin Configuration.

Figure 6
Select the Pin Settings tab and sort the entries by Ports, as shown in Figure 7.

Figure 7
Now, select the Pin Settings tab and then scroll down to the SERCOM5 module as follows:
- Enable I²C Data (I²C_SDA) (SERCOM5_PAD0) on PB30 (Pin #95) as Secure mode.
- Enable I²C Clock (I²C_SCL) (SERCOM5_PAD1) on PB31 (Pin #96) as Secure mode.

Figure 8
This completes the configuration of the I²C peripheral library. The application code will use the I²C PLIB Application Programming Interfaces (APIs) to read temperature from the temperature sensor.
Configure the Non-Secure Universal Synchronous Asynchronous Receiver Transmitter (USART) Peripheral Library and USART pins.
Under the tab Device Resources tab, expand Harmony > Peripheral > SERCOM.
Double-click on SERCOM3 to add the SERCOM instance 3 to the project.

Figure 9
Select the SERCOM3 Peripheral Library in the Project Graph and verify default SERCOM Operation Mode configuration is set as USART. Configure it as shown in Figure 10.

Figure 10
Verify the default baud rate is set to 115200 Hz.
Select the Pin Settings tab and then scroll down to the SERCOM3 module.
- Enable USART_TX (SERCOM3_PAD0) on PB20 (Pin #68) as NonSecure Mode.
- Enable USART_RX (SERCOM3_PAD1) on PB21 (Pin #69) as NonSecure Mode.

Figure 11
Configure the Non-Secure DMA Peripheral Library.
Open the DMA Configuration tabs by clicking Project Graph > Plugins > DMA Configuration

Figure 12
Click on the DMA Settings tab.
Configure DMA Channel 0 to transmit application buffer to the USART TX register. The DMA transfers one byte from the user buffer to USART transmit buffer on each trigger.
- Configure DMA Channel 1 to receive the USART RX register data to application receive buffer. The DMA transfers one byte from the USART receive buffer to the user buffer on each trigger.
Based on the trigger source, the DMA channels configuration is automatically set by MPLAB Code Configurator (MCC).
- Trigger Action: Action taken by DMA on receiving a trigger.
- One beat transfer: Generally used during a memory-to-peripheral or peripheral-to-memory transfer.
- One block transfer: Generally used during the memory-to-memory transfer on a software trigger.
- Source Address Mode, Destination Address Mode: Select whether to increment Source/Destination Address after every transfer. Automatically set by MCC based on the trigger type. For example:
- If the trigger source is USART transmit, then the Source Address is incremented, and the Destination Address is fixed.
- If the trigger source is USART receive, then the Source Address is fixed, and the Destination Address is incremented.
- Beat Size: Size of one beat. The default value is 8 bits. For example:
- If the Serial Peripheral Interface (SPI) peripheral is configured for 16-bit/32-bit mode, then the beat size must be set to 16-bits/32-bits respectively.
Click on Add Channel to add DMA channels and configure the DMA channels.

Figure 13

Figure 14
Launch NVIC Configuration by selecting Project Graph > Plugins > NVIC Configuration.

Figure 15
Click on the NVIC Settings tab. Verify that the DMAC_0 (DMA Channel 0) and DMAC_1 (DMA Channel 1) as NON-SECURE projects.

Figure 16