Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Loadable Setup in the Project Window of the MPLAB® X IDE
Last modified by Microchip on 2024/06/24 06:33
Where to Find Loadables in the Project Window
Right-click on the "Loadables" folder in the Projects window (see accompanying image) and select an option:
"Add Loadable Project" – select to add an existing project to your current project. Repeat to add additional projects.
"Add Loadable Files" – select to add an existing hex file to your current project. Repeat to add additional hex files.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.