Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Loading Different Setups in the Project Properties Window of the MPLAB X IDE
Last modified by Microchip on 2024/06/24 06:33
Loading a Setup in the Project Properties Window
Open the Project Properties window (File > Project Properties) and click on Loading.
Loading an Alternative Hex File
Click to check “Load this .hex file instead of …”.
The next time you build the current project, the alternative hex file will load on build complete.
Loading Debug Symbols During Program/Build
The checkbox to “Load symbols when programming or building for production (slows process)” allows you to load debug symbols when programming, as when using RTDM with DMCI, Motor Control applications, etc. Otherwise, the checkbox should be left unchecked to speed up programming and building (default).
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.