Favorites Window Usage in the MPLAB® X IDE
Last modified by Microchip on 2024/06/24 06:33
What is the Favorites Window?
The Favorites window enables the user to access any file on the computer or network within the MPLAB® X IDE environment without having to create a project for that file. This is especially useful when you want to access a file outside of the project.
The Favorites window can be accessed by choosing Window > Favorites.

When the Favorites window is first opened, it contains the computer's home directory only. You can add any folder/file by right-clicking on the window and choosing Add to Favorites….