What's new in XWiki
XWiki and Cryptpad communities meetup at FOSDEM 2025
2025/01/20 16:18
The XWiki development team is happy to announce that the XWiki and CryptPad communities will be gathering at an informal meetup at FOSDEM, on Saturday, 1st of February. For this purpose, we have created a registration form so that we can organize everything and also keep you informed of all the latest details.
Important information to know:
- Day: February 1, 2025
- Hour: starting with 20:00 until 00:00
- Location: Scott’s Bar & Kitchen, Rue Montagne aux Herbes Potagères 2,1000 Bruxelles, Belgium
The party will be organized in collaboration with NextCloud and OpenProject.
PS: If by chance you can’t make it anymore, please let us know as soon as possible to open up your place to somebody on the waiting list.
XWiki 15.10.16 Released
2025/01/14 21:00
The XWiki development team is proud to announce the availability of XWiki 15.10.16. This is a bug fix release. It contains security fixes, with the highest severity being 9.3/10.0. See the release notes for more information.
XWiki 16.10.2 Released
2024/12/25 19:04
The XWiki development team is proud to announce the availability of XWiki 16.10.1. This is a bug fix release, but it also marks the beginning of 16.10.x as the LTS branch. This release also includes security fixes. See the release notes for more information.
XWiki 16.10.1 Released
2024/12/09 17:54
The XWiki development team is proud to announce the availability of XWiki 16.10.1. This is a bug fix release including security fixes. See the release notes for more information.
XWiki 15.10.15 Released
2024/12/05 03:14
The XWiki development team is proud to announce the availability of XWiki 15.0.15. This is a bug fix release. It contains security fixes, with the highest severity being 7.9/10.0. See the release notes for more information.
Numbered Content 1.10.3 Released
2024/12/04 23:55
Numbered Content 1.10.3 has been released. This is a bugfix release.
XWiki 16.10.0 Released
2024/11/28 17:13
The XWiki development team is proud to announce the availability of XWiki 16.10.0. This release comes with two usability improvements: the authentication process is now easier to discover, and editing the avatar in the user profile is now easier. Is also brings minor accessibility improvements, as well as technical modules that will be useful to improve security in the future. This release contains security fixes, with the highest severity being 8.7/10. See the release notes for more information.
Sync macro 1.0 released
2024/11/18 03:52
The first version of the Sync Macro was released. See more details on how to use it on Sync Macro extension page.
XWiki 15.10.14 Released
2024/11/17 19:05
The XWiki development team is proud to announce the availability of XWiki 15.10.14. This release is a bug fix release. This release contains security fixes, with the highest severity being 8.7/10.0. See the release notes for more information.
A hands-on guide to migrating from Confluence - why it’s more than just a technical shift
2024/11/17 16:00
Discover how migrating from Confluence to XWiki can transform your team's collaboration. Learn about the benefits of open-source freedom, complete data ownership, and flexible customization. XWiki SAS's expert-built Confluence Migration Toolkit ensures a seamless transition with minimal disruptions, backed by continuous support and evolving tools. Ready to make the switch? Join XWiki SAS's webinar!
XWiki 16.9.0 Released
2024/10/27 20:17
The XWiki development team is proud to announce the availability of XWiki 16.9.0. This release enables realtime WYSIWYG editing by default and contains a number of smaller improvements and bug fixes. See the release notes for more information.
🤖 The first AI-assistant in XWiki is here! (BETA)
2024/10/09 15:00
XWiki SAS announces the release of the first XWiki LLM application (BETA), funded by NGI Search. The app integrates AI-powered functionalities directly into your wiki instance, bringing content generation, translation, and intelligent knowledge retrieval to your fingertips. To facilitate this, we’ve integrated a chatbot inside XWiki that allows you to ask any question about the information in your wiki, receiving answers based on our Retrieval Augmented Generation (RAG) system. Additionally, the LLM app offers you flexibility and control over your data through the chosen model, ensuring that your sensitive information remains private and secure. Read the full announcement here.
Introducing our new Confluence Migration Toolkit and 3 most requested bridge macros
2024/08/05 15:00
XWiki SAS has launched 3 Confluence-equivalent bridge macros — Page Properties, Page Properties Report, and Content by Label. These macros can be found in the new Confluence Migration Toolkit, a bundle with all the macros, apps, and services that you need to transfer data but also benefit from long-term technical support from XWiki SAS. Read the full announcement here.
Open letter to the European Commission
2024/07/16 15:00
The XWiki SAS and CryptPad development teams support this open letter addressed to the European Commission in favor of funding the Next Generation Internet (NGI) programs. The letter emphasizes the critical role the programs have in supporting open-source software development and technological innovation, calling for the preservation of NGI to maintain digital sovereignty and foster long-term international collaborations. Read the full article here.
Run your on-prem wiki instance like a pro with Admin Tools Application (Pro)
2024/06/18 15:00
XWiki SAS has released the Admin Tools Application (Pro) v1.0, one of the many business-ready Pro Apps, available in the XWiki SAS store. Through this app, you can optimize your XWiki on-prem installation, maintenance, and resources allocation — all from one central dashboard. Read the full article here.
Matomo integration in your wiki with Analytics Application (Pro)
2024/05/15 15:00
XWiki SAS has released the Analytics Application (Pro) v1.0, one of the many business-ready Pro Apps, available in the XWiki SAS store. Through this app, you can learn valuable insights about the most accessed pages, searched terms and user behavior from your company wiki or public website — all straight from your XWiki instance. This way, you'll have an open-source ecosystem without any data lock-in. Read the full article here.
Enhancing digital sovereignty: XWiki and Nextcloud forge closer ties
2024/03/06 16:00
XWiki SAS has long upheld its commitment to independence, with shareholders exclusively comprising current and former employees. However, recognizing the importance of strong collaboration among major open-source projects in the EU, the company is embracing a strategic shift through a symbolic investment in XWiki SAS from Frank Karlitschek, Founder and CEO of Nextcloud. Moreover, Nextcloud GmbH and XWiki SAS have signed a mutual resellers' agreement to provide their customers an easy way to purchase a complete solution from either vendor. Read the full article to learn about the why, how, and what.
New in XWiki Cloud, now updated to 15.5.4
2024/02/21 16:00
XWiki SAS has upgraded XWiki Cloud to version 15.5.4 of XWiki. XWiki Cloud is a convenient and cost-effective solution for running XWiki. XWiki SAS handles the setup, hosting, upgrades, maintenance, and backups, allowing you to focus on your work. To try out all the new features and improvements, set up a Cloud demo in just a few minutes.
Confluence Migrator (Pro): streamlined multi space import and new improved UI
2023/09/27 15:00
XWiki SAS has launched the new Confluence Migrator (Pro), an all-in-one toolkit that allows you to quickly migrate and reorganize your content in the hierarchical order identically as to how it was on the Confluence side. The migrator is available for any deployment method, whether it is on your premise or in the XWiki Cloud. Read the full article to learn about all its new features and how to install it.
Improvements and features to try in XWiki 15.x
2023/07/30 15:00
XWiki SAS did a short mid-year recap of the most notable features and improvements done so far in the 15.x cycle of development by the XWiki SAS Product team and the XWiki community contributors. Read the full article here.