Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Open the Project Properties Window in MPLAB X IDE
Last modified by Microchip on 2024/06/24 06:34
Three Methods for Opening the Project Properties
The Project Properties Window is a utility to allow you to modify project parameters. There are three methods you can use to open the project properties window.
From the Projects Window
Right click on the top node of the project ()
Select Properties from the bottom of the very tall pop-up menu.
From the File Menu
From the main menu, select File > Project Properties(ProjectName) where ProjectName is the name of the project whose properties you want to view.
If you have multiple projects open, you should see one entry in the File menu for each of them.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.