Dashboard Operations in the MPLAB® X IDE
What is the Dashboard?
The Project Dashboard contains information about the current project which can be useful to the developer. This page shows how to open the Dashboard and extract the data.
Items Found on the Dashboard Border

When pressed, this icon will open up the Project Properties window
This icon will cause the IDE to update the connection status of the selected debug tool
Alternately disables or enables the breakpoint.
Opens up a link to a web-based version of the datasheet, in PDF form, for the MCU being used
Opens up the help file for the compiler being used
Opening the Dashboard
From MPLAB® X IDE's main toolbar Select Window > Dashboard
Unless it has been specifically moved in a previous setting, the Dashboard Window will open in the lower left-hand corner of the IDE.

What's Found Inside the Dashboard?

Once a project has been built the Dashboard Window will display the following information:
- MCU
- Program Checksum
- Build Tool
- Memory Usage
- Debug Resources
- Debug Tool