Customizing the Main Toolbar of the MPLAB® X IDE
Adding Icons to a Toolbar Group
Selecting View > Toolbar > Customize will open the Customize Toolbar window. The Customize Toolbar window displays the list of the icons which can be placed on the toolbar.
To add an icon to a group, select an item from the list on the Customize Toolbar window and drag it onto the desired Toolbar group.
Removing Icons From a Toolbar Group
Open the Customize Toolbar Window by selecting View > Toolbar > Customize.
Select the icon from the toolbar then drag it off the toolbar. When an icon is dragged off the toolbar a small trash can will appear. Unselecting the icon while the trash can is visible removes the icon from the toolbar
Customizing a Group of Icons
Open the Customize Toolbar Window by selecting View > Toolbar > Customize.
Select the New Toolbar button.
Name your new toolbar then select OK.
Your new toolbar group will appear in the main toolbar. Add icons to your new group using the same steps taken to add icons to the default groups.
Resetting the Toolbar
Selecting View > Toolbar > Reset Toolbars will cause the toolbar to return to its default configuration.