MPLAB® IPE Window Menu
Last modified by Microchip on 2023/11/09 09:10
The Window Menu can be found at the top of the MPLAB® Integrated Programming Environment (IPE). The Window menu options are:
- Output
- Target Memory Device
- Reset Windows
Output
This option opens the Output window at the bottom of the display. Right-click the tab title to display window options, such as Close, Float, Move, etc.
Right-click in the body of the window to display Output window content options, such as Find, Wrap text, etc.

Target Memory Views
This option is available only if Production Settings are set in Advanced Mode to view the different types of memory. Some of the possible memory views include Program Memory, Configuration Bits, User ID Memory, Device ID Memory, etc.

Reset Windows
Selecting this option will reset all the program windows to the default settings.