Console UART Functionality of the SAMA5D2 Series Arm® Cortex®-A5 Microprocessor Unit (MPU) in the Linux® Kernel
Introduction
This training topic shows how to configure the Console Universal Asynchronous Receiver Transmitter (UART) functionality of the SAMA5D2 Series Arm® Cortex®-A5 Microprocessor Unit (MPU) in the Linux® kernel.
The default Console UART configuration for the ATSAMA5D27-SOM1-EK1 is UART1, which is connected to the J-LINK-OB microprocessor U4, which in turn provides a Serial-to-USB conversion to the micro-USB connector J10. In this topic, you will switch the Console UART from UART1 to UART2 and access the Console UART from the mikroBUS™ 2 expansion socket.
Recall that the Boot Process for the SAMA5D2 Series MPUs follows the order of:
- ROM Boot Code
- at91bootstrap
- u-boot-at91
- linux-at91
Each of the steps has configuration information that points it to the specified Console UART. In order to switch the Console UART from UART1 to UART2, you will have to alter the default configuration files and Device Trees. We show you how in this training topic.
Prerequisites
This application is developed for the ATSAMA5D27-SOM1-EK1 development platform:
This application is developed using the Buildroot build system.
Hardware
For this application, you will be switching the console UART from UART1 to UART2 on the ATSAMA5D27-SOM1-EK1 Evaluation Kit.
UART1
The ATSAMA5D27 SOM1 contains five UART peripherals to provide two-pin serial communications. By default, the console UART is configured to UART1 which connects to the U4 J-Link-OB microcontroller and the J10 micro-USB connector. The U4 J-Link-OB provides an onboard Serial-to-USB converter.
The figures below show the debugging capabilities of the SOM1-EK1 and a snippet of the schematic diagram of UART1.

| Schematic Name | UART1 | Package Pin |
|---|---|---|
| DBUG_RXD | URXD1 | PD2 |
| DBUG_TXD | UTXD1 | PD3 |

UART2 on mikroBUS
You will control the UART2 peripheral from the ATSAMA5D27 SOM1 on the mikroBUS 2 expansion socket.
The figures below show the expansion capability of the SOM1-EK1 and a snippet of the schematic for the mikroBUS 2 connectors.

| mikroBUS 2 pin | Schematic Name | UART2 | Package Pin |
|---|---|---|---|
| J30 pin 3 | RX_mBUS2 | URXD2 | PD23 |
| J30 pin 4 | TX_mBUS2 | UTXD2 | PD24 |
mikroBUS 2

Buildroot Configuration
Objective: Using Buildroot, build a bootable image and Flash it onto an SD memory card for the ATSAMA5D27-SOM1-EK1 development board.
Follow the steps for building the image on the "Buildroot - Create Project with Default Configuration" page. In the topic, you will use the default configuration file: atmel_sama5d27_som1_ek_mmc_dev_defconfig
In order to switch the Console UART from UART1 to UART2, changes are required for each of the stages of the Boot Process. We show you below the changes you will need to make.
at91bootstrap3
Objective: Change the Debug Unit (DBGU) Settings in the file: buildroot-at91/output/build/at91bootstrap3-v3.8.12/board/sama5d27_som1_ek/sama5d27_som1_ek.h
* DBGU Settings
*/
#define USART_BASE AT91C_BASE_UART2
#define CONFIG_SYS_DBGU_RXD_PIN AT91C_PIN_PD(23)
#define CONFIG_SYS_DBGU_TXD_PIN AT91C_PIN_PD(24)
#define CONFIG_SYS_DBGU_ID AT91C_ID_UART2
u-boot-at91
Objective: Change the following definitions in the file: buildroot-at91/output/build/uboot-linux4sam_6.0/arch/arm/dts/at91-sama5d27_som1_ek.dts
53 u-boot,dm-pre-reloc;
54 stdout-path = &uart2;
55 };
.
.
124 uart2: serial@f8024000 {
125 pinctrl-names = "default";
126 pinctrl-0 = <&pinctrl_uart2_default>;
127 status = "okay";
128 u-boot,dm-pre-reloc;
129 };
.
.
207 pinctrl_uart2_default: uart2_default {
208 pinmux = <PIN_PD23__URXD2>,
209 <PIN_PD24__UTXD2>;
210 bias-disable;
211 u-boot,dm-pre-reloc;
212 };
Line 54 change the stdout-path from uart1 to uart2.
Line 124 change definitions from uart1 to uart2.
Line 127 enable uart2.
Line 207 change definitions from uart1 to uart2.
Objective: Add the following lines of code in the file: buildroot-at91/output/build/uboot-linux4sam_6.0/board/atmel/sama5d27_som1_ek/sama5d27_som1_ek.c
39 static void board_uart1_hw_init(void)
40 {
41 atmel_pio4_set_a_periph(AT91_PIO_PORTD, 2, ATMEL_PIO_PUEN_MASK); /* URXD1 */
42 atmel_pio4_set_a_periph(AT91_PIO_PORTD, 3, 0); /* UTXD1 */
43
44 at91_periph_clk_enable(ATMEL_ID_UART1);
45 }
46
46a static void board_uart2_hw_init(void)
46b {
46c atmel_pio4_set_a_periph(AT91_PIO_PORTD, 23, ATMEL_PIO_PUEN_MASK); /* URXD2 */
46d atmel_pio4_set_a_periph(AT91_PIO_PORTD, 24, 0); /* UTXD2 */
46e
46f at91_periph_clk_enable(ATMEL_ID_UART2);
46g }
46h
47 void board_debug_uart_init(void)
48 {
49 board_uart2_hw_init();
50 }
51 #endif
Lines 46a through 46h add the following lines of code to initialize uart2 hardware.
Line 49 change uart1 to uart2 to call the initialization of the uart2 hardware.
Objective: Change the following definitions in the file: buildroot-at91/output/build/uboot-linux4sam_6.0/configs/sama5d27_som1_ek_mmc_defconfig
.
.
26 CONFIG_BOOTARGS="console=ttyS2,115200 earlyprintk root=/dev/mmcblk0p2 rw rootwait"
Line 14 change CONFIG_DEBUG_UART_BASE from 0xf8020000 to 0xf8024000.
Line 26 change CONFIG_BOOTARGS console from ttyS0 to ttyS2
Kernel
The Buildroot default configuration file: atmel_sama5d27_som1_ek_mmc_dev_defconfig has UART2 enabled in the Linux Kernel. Therefore, there are no changes required in the kernel.
Objective: Observe the UART2 definitions in the file: buildroot-at91/output/build/uboot-linux4sam_6.0/arch/arm/dts/at91-sama5d27_som1_ek.dts
57 serial0 = &uart1; /* DBGU */
58 serial1 = &uart4; /* mikro BUS 1 */
59 serial2 = &uart2; /* mikro BUS 2 */
60 i2c1 = &i2c1;
61 i2c2 = &i2c2;
62 };
.
.
165 uart2: serial@f8024000 {
166 pinctrl-names = "default";
167 pinctrl-0 = <&pinctrl_mikrobus2_uart>;
168 atmel,use-dma-rx;
169 atmel,use-dma-tx;
170 status = "okay";
171 };
.
.
516 pinctrl_mikrobus2_uart: mikrobus2_uart {
517 pinmux = <PIN_PD23__URXD2>,
518 <PIN_PD24__UTXD2>;
519 bias-disable;
520 };
Line 59 shows the alias of uart2 is serial2; uart2 will be registered as ttyS2.
Line 170 shows uart2 was enabled with the default setting
Line 517 shows PD23 and PD24 were selected for uart2 on mikroBUS 2.
RomBOOT
The console UART can be changed during RomBOOT. Refer to "Section 16", "Standard Boot Strategies" in the SAMA5D2 Series Datasheet (DS60001476). The Boot Configuration Word UART_CONSOLE bits select the pins and UART interface used for the console.

The Boot Configuration Word can be updated by SAM-BA® In-System Programmer (ISP). Here is a command example:
Connection
For the Hands-On portion of this topic, connect a Serial-to-USB converter (TTL level) to UART2 on the mikroBUS 2 expansion slot to your PC.
| mikroBUS 2 pin | Schematic Name | Serial-to-USB Adapter |
|---|---|---|
| J30 pin 3 | RX_mBUS2 | TXD |
| J30 pin 4 | TX_mBUS2 | RXD |

Hands-On
Run your favorite terminal emulation program on your PC to view the booting sequence on the newly assigned console UART.

Summary
In this topic, you reconfigured the Console UART to UART2 in the at91bootstrap3, u-boot-at91, and kernel. You viewed the system boot-up while connected to UART2 on the mikroBUS 2 expansion slot.