SAM9X60-EK Evaluation Kit - Booting from NAND Flash Memory
- Prerequisites
- Hardware
- SAM-BA In-System Programmer
- Erase NAND Flash Memory
- Build at91bootstrap and Write to NAND Flash Memory
- Build u-boot-at91 and Write to NAND Flash Memory
- Create u-boot-env.bin and Write to NAND Flash Memory
- Build the Linux® Kernel Image and Device Tree Blob (DTB)
- Create Flattened Image Tree (FIT) and Write to NAND Flash Memory
- Prepare a Root File System (ROOTFS) for NAND Flash Memory
- Boot from NAND Flash Memory
- Summary
- Learn More
Prerequisites
- Familiar with the features of the SAM9X60-EK Evaluation Kit
- A working cross-toolchain for Arm®-based MPU target
- Familiar with the operation of the SAM-BA® In-System Programmer
- Setup Console Serial Communications for the SAM9X60-EK
- Knowledge of the Boot Process:
- SAM9X60 Boot Process
- SAM9X60 Datasheet (Section 12 – Boot Strategies)
Hardware

For this training topic, you will be using the SAM9X60-EK Evaluation Kit. You will also need two USB Micro-B cables. One cable will connect the Host PC to the target console to view the SAM-BA Monitor log message. The second cable will connect the Host PC to the target USBA port (J7) so that the SAM-BA Host can communicate with the SAM-BA Monitor.
Bootable Memory
The SAM9X60-EK Evaluation Kit has a 4 Gb (512 M x 8) NAND Flash memory (U9) (Micron MT29F4G08ABAEA) that may be used for booting an embedded Linux® system.

You will configure and build bootable files at91bootstrap, u-boot-at91, Flattened Image Tree (FIT) (containing the Linux kernel and device tree), and Root File System (RFS) to be Flashed into U9 using the SAM-BA In-System Programmer (ISP).

SAM-BA In-System Programmer
In this section, you will load the SAM-BA Host Application (if you have not already done so) and set up Console and SAM-BA Host to Monitor communications.
Setup SAM9X60-EK Console Serial Communications
To view the SAM-BA Monitor log messages, set up console serial communications following the instructions on the "SAM9X60-EK Evaluation Kit - Console Serial Communications" page.
You have two choices in connecting to a serial port on the SAM9X60-EK:
- The first is using a USB cable to connect to the J-LINK-OB port (J22). This method has the added benefit of powering the SAM9X60-EK.
- The second is using a USB-to-TTL converter to connect to the Universal Asynchronous Receiver Transmitter (UART) Debug port (J24). With this option, to power the SAM9X60-EK, you will need to:
- Use an external 5 VDC power supply connected to J1 (coaxial power jack), or
- Use a USB cable connected to the USBA port (J7). As you’ll be connecting a USB cable in Step 3 below (SAM-BA Host to Monitor Communications), this is the easiest method.


If it is not already installed, install the SAM-BA Host Application.
Setup the SAM-BA Host to Monitor Serial Communications
With SAM-BA Monitor on the target, you must have installed the SAM-BA Host on a Linux PC (Step 2 above), and connect a USB Micro-B cable from the host PC to the USBA port (J7) on the SAM9X60-EK as shown in the accompanying figure.

Ensure there is no SD memory card inserted in slot J4.
Open Jumper the DISABLE_BOOT (J13).
This will allow booting from the onboard memories (NAND and QSPI Flash).
Press both the DIS_BOOT (SW4) and RESET (SW3) push buttons.
Pressing the DIS_BOOT (SW4) push button disables booting from the onboard memories.
Continue pressing the DIS_BOOT(SW4) while releasing the RESET (SW3) push button.
The SAM9X60-EK will boot to the SAM-BA Monitor and start communications with the SAM-BA Host. Observe ROMBoot on the Console (terminal emulator) indicating the SAM-BA Monitor is running.
Erase NAND Flash Memory
In this section, you will erase the contents of the NAND Flash Memory located on the SAM9X60-EK. This is a necessary step before writing data to the NAND Flash Memory.
Erase NAND Flash Memory
Erase the contents of the NAND Flash Memory on the SAM9X60-EK with the following command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 8192 bytes (2 pages) at address 0x0030aca0.
NAND header value is 0xc1e04e07.
Supported erase block size: 256KB
Executing command 'erase'
Erased 262144 bytes at address 0x00000000 (0.05%)
Erased 262144 bytes at address 0x00040000 (0.10%)
..
..
Erased 262144 bytes at address 0x1ff80000 (99.95%)
Erased 262144 bytes at address 0x1ffc0000 (100.00%)
Connection closed.
Build at91bootstrap and Write to NAND Flash Memory
In this section, you will configure and build the second-stage bootloader, at91bootstrap, from source code to boot from NAND Flash Memory and write it to NAND Flash Memory.
For more information, including how to download, see the "at91bootstrap: A Second Stage Bootloader for Microchip Microprocessors" training.
Change directory into the at91bootstrap directory:
Using a default configuration file, configure at91bootstrap to boot u-boot from NAND Flash Memory:
# CLEAN obj and misc files!
# CLEAN configuration files!
# CLEAN binary files!
$ make sam9x60eknf_uboot_defconfig
#
# configuration written to .config
#
#
# make dependencies written to .auto.deps
# See top of this file before playing with this auto-prerequisites!
#
Optional: If you would like to verify the NAND Flash Memory settings or make any customizations:

Observe that Board Type (sam9X60ek) has been selected.
Highlight Memory selection ---> and press ENTER.
Highlight NAND flash configuration ---> and press ENTER.
You can see the default NAND flash configuration set for SAM9X60-EK.

You may exit menuconfig by repeatedly typing "ESC-ESC" until it closes. Do not save any changes.
Build at91bootstrap:
Once the build is complete, the resulting binary files are in the ~/at91bootstrap/binaries/ directory:
$ ls
at91bootstrap.bin
boot.bin
sam9x60ek-nandflashboot—uboot-3.9.2.bin
sam9x60ek-nandflashboot—uboot-3.9.2.bin.pmecc
sam9x60ek-nandflashboot-uboot—3.9.2.elf
sam9x60ek-nandflashboot-uboot—3.9.2.map
From the SAM-BA Host command line, write at91bootstrap.bin to NAND Flash Memory starting at location 0x0 using the nandflash applet writeboot command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 8192 bytes (2 pages) at address 0x0030aca0.
NAND header value is 0xc1e04e07.
Supported erase block size: 256KB
Executing command 'write:at91bootstrap.bin'
Appending 3588 bytes of padding to fill the last written page
Wrote 8192 bytes at address 0x00000000 (50%)
Wrote 8192 bytes at address 0x00002000 (100%)
Connection closed.
The result is at91bootstrap.bin is stored in the NAND Flash Memory starting at address 0x0.

Build u-boot-at91 and Write to NAND Flash Memory
In this section, you will configure and build the third-stage bootloader, u-boot-at91, from source code to boot from NAND Flash Memory and write it to NAND Flash Memory.
Change directory to your working directory containing the u-boot-at91:
Using a default configuration file, configure u-boot-at91 for NAND Flash Memory:
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
HOSTCC scripts/kconfig/zconf.tab.o
HOSTLD scripts/kconfig/conf
#
# configuration written .config
#
Optional: If you would like to verify settings for booting from NAND Flash Memory or make any customizations, type:

Highlight Boot media > and press ENTER.
[*] Support for booting from NAND flash ---> has been selected.
You may exit menuconfig by repeatedly typing "ESC-ESC" until it closes. Do not save any changes.
Build u-boot-at91:
Once the build is complete, the resulting binary file u-boot.bin is in the u-boot-at91 directory.
From the SAM-BA Host command line, write u-boot.bin to NAND Flash Memory starting at location 0x40000 using the applet -a nandflash -c write command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 8192 bytes (2 pages) at address 0x0030aca0.
NAND header value is 0xc1e04e07.
Supported erase block size: 256KB
Executing command 'write:u-boot.bin:0x40000'
Appending 2794 bytes of padding to fill the last written page
Wrote 8192 bytes at address 0x00040000 (1.41%)
Wrote 8192 bytes at address 0x00042000 (2.82%)
…
…
Wrote 8192 bytes at address 0x000ca000 (98.59%)
Wrote 8192 bytes at address 0x000cc000 (100%)
Connection closed.
The result is u-boot.bin is stored on the NAND Flash Memory starting at address 0x40000.

Create u-boot-env.bin and Write to NAND Flash Memory
Configuration of U-Boot is performed using environment variables. They are stored in binary format, generally, on the same boot memory (mass storage) that U-Boot is stored.
In this section, you will create a U-Boot environment binary file by first creating a text file. The text file is then converted to binary format using a utility program, mkenvimage. Finally, you will write the file to NAND Flash Memory using the SAM-BA In-System Programmer (ISP).
Using your favorite text editor, create a text file with the following information. Name the text file u-boot-env.txt.
bootargs=console=ttyS0,115200 mtdparts=atmel_nand:256k(bootstrap)ro,768k(uboot)ro,256k(env_redundant),256k(env),6656k(itb)ro,
-(rootfs) rootfstype=ubifs ubi.mtd=11 root=ubi0:rootfs rw atmel.pm_modes=standby,ulp0
bootcmd=nand read 0x24000000 0x00180000 0x49b46c; bootm 0x24000000#kernel_dtb
bootdelay=1
stderr=serial
stdin=serial
stdout=serial
The bootargs line tells U-Boot:
- The console= device and baud
- The root= location of the root filesystem and permissions
- The rootfstype= root filesystem type
The bootcmd= line tells U-Boot to load the sam9x60ek.itb file from address 0x00180000 of NAND Flash memory to external DDR2 SDRAM starting at address 0x24000000.
Convert the text file u-boot-env.txt into a binary file u-boot-env.bin using the utility program mkenvimage.
From the SAM-BA Host command line, write u-boot-env.bin to NAND Flash Memory starting at location 0x140000 using the applet -a nandflash -c write command:
The result is u-boot environment is stored in the NAND Flash Memory starting at address 0x40000.

Build the Linux® Kernel Image and Device Tree Blob (DTB)
In this section, you will configure the Linux kernel and device tree for the SAM9X60-EK evaluation kit using the default configuration and build files. In the next section, you will use these files to create a Flattened Image Tree (FIT) image and write it to NAND Flash Memory.
Change the directory to your working directory containing the linux-at91 source code:
Using default configuration files, configure the Linux kernel using the following command:
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
HOSTCC scripts/kconfig/confdata.o
HOSTCC scripts/kconfig/expr.o
LEX scripts/kconfig/lexer.lex.c
YACC scripts/kconfig/parser.tab.[ch]
HOSTCC scripts/kconfig/lexer/lex.o
HOSTCC scripts/kconfig/parser.tab.o
HOSTCC scripts/kconfig/preprocess.o
HOSTCC scripts/kconfig/symbol.o
HOSTLD scripts/kconfig/conf
#
# configuration written to .config
#
Optional: If you would like to verify settings or make customization changes type:

You may exit menuconfig by repeatedly typing "ESC-ESC" until it closes. Do not save any changes.
Build linux-at91:
Once the build is complete, the resulting binary files are created:
/arch/arm/boot/dts/at91-sam9x60ek.dtb
Create Flattened Image Tree (FIT) and Write to NAND Flash Memory
In this section, you will create a Flattened Image Tree (FIT). The FIT image allows for more flexibility in handling images of various types and enhances the integrity protection of images with stronger checksums. An Image Source (*.its) file and a set of data files are used as input. An Image Tree Blob (*.itb) file is generated as the output. Finally, you will write the FIT image to NAND Flash Memory.
Git clone the Device Tree Overlay files from the Linux4SAM repository:
Change directory to your working directory containing the dt-overlay-at91:
Open Makefile with your favorite editor and verify that the KERNEL_DIR is pointing to your linux-at91 directory:
DTC_OPTIONS?=-@
DTC_OPTIONS += -Wno-unit_address_vs_reg -Wno-graph_child_address -Wno_pwms_property
KERNEL_DIR?=../linux-at91 <--- Ensure pointing to your linux-at91 directory
KERNEL_BUILD_DIR?=$(KERNEL_DIR)
DTC?=$(KERNEL_BUILD_DIR)/scripts/dtc/dtc
Or you can set the KERNEL_DIR environment variable:
$ export KERNEL_DIR=path
$ echo $KERNEL_DIR
Build the *.itb image file:
Once the build is complete, the resulting image file sam9x60ek.itb is located in the dt-overlay-at91 directory.
Write Image Tree Blob (ITB) to NAND Flash Memory using the following command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 8192 bytes (2 pages) at address 0x0030aca0.
NAND header value is 0xc1e04e07.
Supported erase block size: 256KB
Executing command 'write:sam9x60ek.itb:0x180000'
Wrote 8192 bytes at address 0x00180000 (0.17%)
Wrote 8192 bytes at address 0x00142000 (0.34%)
…
…
Wrote 8192 bytes at address 0x0015c000 (99.83%)
Wrote 8192 bytes at address 0x0015e000 (100%)
Connection closed.
The result is the Flattened Image Tree (FIT) is stored in the NAND Flash Memory starting at address 0x180000.
Prepare a Root File System (ROOTFS) for NAND Flash Memory
In this section, you will download a demonstration image from the Linux4SAM website to use the ROOTFS on the image. You will Flash the image to NAND Flash Memory.
Download the SAM9X60-EK demonstration package from the Linux4SAM website.
Download and extract the linux4sam-poky-sam9x60ek-headless-2020.04.zip file.
Flash the RootFS image to NAND Flash Memory.
Once you have the package extracted, you will use the microchip-headless-image-sam9x60ek.ubi file. This is the RootFS in the Unsorted Block Image File System (UBIFS) format.
Write to NAND Flash Memory using the following command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 8192 bytes (2 pages) at address 0x0030aca0.
NAND header value is 0xc1e04e07.
Supported erase block size: 256KB
Executing command 'write:microchip-headless-image-sam9x60ek.ubi:0x800000'
Wrote 8192 bytes at address 0x00800000 (0.01%)
Wrote 8192 bytes at address 0x00802000 (0.01%)
…
…
Wrote 8192 bytes at address 0x0015c000 (99.83%)
Wrote 8192 bytes at address 0x0015e000 (100%)
Connection closed.
The result is the Root File System is stored in the NAND Flash Memory starting at address 0x800000.
Boot from NAND Flash Memory
Check that you have Console Serial Communications established.
Review STEP 1 of the SAM-BA In-System Programmer section above.
Check that jumper the DIS_BOOT (J13) is open.
This will allow booting from the onboard memories (NAND and QSPI Flash).
Press the RESET button SW3 (nRST).
The boot log will be displayed in the terminal emulator. In the end, the command line will prompt the user to log in. Login as ‘root’. There is no password required to log in.
Proper operation of the image will be indicated by a flashing blue RGB LED (LD1).
If Console Serial Communications is connected to J22, the operation of the onboard J-Link Debugger will be indicated by a flashing green LED (D9).
Congratulations! You have created an embedded Linux system that boots from NAND Flash memory.
Summary
In this training topic, you configured and built the second-stage bootloader at91bootstap, the third-stage bootloader u-boot-at91, Linux kernel, and device tree. You created a Flattened Image Tree (FIT) containing the Linux kernel and device tree. You prepared a Root File System (RootFS) in the UBIFS format from a Linux4SAM demonstration image. Each of these you individually wrote to NAND Flash Memory. The result is an embedded Linux system that boots from NAND Flash Memory.