SAM9X60-EK Evaluation Kit - Features

Last modified by Microchip on 2025/09/10 14:53

Introduction

Photograph of the SAM9X60-EK

In this training, we described the features of the SAM9X60-EK evaluation kit with links to additional information.

Unfortunately, the SAM9X60-EK Evaluation Kit is no longer in production due to memory components that have been obsoleted. For those new to the SAM9X60, take a look at the SAM9X60-Curiosity Development Board.

Features Summary

The major features of the SAM9X60-EK evaluation kit are:

Back to top

SAM9X60 MPU

The SAM9X60 is a high-performance, ultra-low-power ARM926EJ-S CPU-based embedded microprocessor (MPU). Its features include:

  • 600 MHz ARM926EJ-S Core
  • 64 KB SRAM
  • LCD Controller
  • 2D Graphics Processor Unit
  • Dual 10/100 Ethernet
  • Dual CAN
  • Camera Interface

Back to top

Mass Storage

There is one mass storage option available on the baseboard.

Mass Storage

Back to top

SD Multimedia Card (SDMMC) (J4)

J4 is a MultiMediaCard (MMC) or Secure Digital (SD) memory card slot. J4 is connected to the SDMMC port 0 (SDMMC0) peripheral of the SAM9X60.

Back to top

Communications

The SAM9X60-EK provides wired communications via Ethernet, USB, CAN. It also has the capability of adding an ATWIL3000 Wi-Fi® plus Bluetooth® module.

Wired and Wireless Communication options

Back to top

Ethernet (J5)

The SAM9X60-EK contains an Ethernet MAC peripheral. It is connected to a 10Base T/100Base-TX Ethernet physical layer transceiver, KSZ8081RNA. A unique EUI-48™ MAC address is provided by a Serial EEPROM, 24AA025E48.

Dual Controller Area Network (CAN) (J6)

The SAM9X60-EK features a dual CAN peripheral J6. It is connected to two MCP2542 transceivers.

Back to top

USB (J7 and J8)

The SAM9X60-EK features three USB communication ports named USB-A, USB-B, and USB-C.

  • The USB-A port acts only as a USB device interface and is accessed via USB Micro-B connector J7.

USB-A (J7) is the default serial port used to communicate with the SAM-BA® Monitor resident on the MPU.

 USB-A (J7) port also acts as a source of power supply to the board. For more information on how to power the baseboard, see the "Power Options" section below.

  • The USB-B and USB-C ports are connected to the stacked USB Type-A connecter (J8). Each port can act both as a device and as a host.

Back to top

Wireless Connectivity

You can add wireless connectivity to the SAM9X60-EK by soldering a ATWILC3000 Wi-Fi/Bluetooth Low Energy module with an integrated chip antenna. ATWILC3000 is a single-chip IEEE 802.11 b/g/n RF/Baseband/MAC link controller and Bluetooth 5 Low Energy.

Back to top

Debugging

There are two methods of debugging the SAM9X60-EK: serial Universal Asynchronous Receiver Transmitter (UART) debug port and JTAG.

Debugging options

Back to top

Serial Debug Port (J24)

The SAM9X60-EK features a dedicated serial port for debugging through J24. You will need a Serial-to-USB adapter to connect the Serial Debug Port to a personal computer.

Back to top

JTAG (J23)

A JTAG interface to the SAM9X60-EK is provided by 20-pin connector J23. This facilitates software development and debugging by connecting an external JTAG debugger.

Back to top

J-Link Onboard (J22)

The baseboard contains an onboard SEGGER J-Link debugger. Microcontroller ATSAM3U4C (U27) and support circuitry contain JTAG and J-Link functionality. U27 provides USB CDC class serial communications via micro-B USB connector J22. This port acts as a power source to the U27 block and is used to program and debug the MPU.

Back to top

Debug Jumpers

J20: Open (default)

J-Link on-board interface is enabled.

J21: Open (default)

UART communication (CDC) between MPU and SAM3U MCU (U27) is enabled.

For more information on all baseboard jumpers, see the "Jumpers" section below.

Back to top

User Interface

User Interface options

Back to top

Audio Class D Connector (J12)

The Audio Class D (CLASSD) Amplifier (J12) is a digital input, Pulse Width Modulation (PWM) output stereo Class D amplifier. The input is compatible with the most common audio data rates. The PWM output can drive either Audio DAC or a Class D power amplifier. Refer to the SAM9X60 datasheet for more information.

Back to top

GPIO/Raspberry Pi Connector(J16)

The SAM9X60-EK contains a 40-pin GPIO connector (J16) for use. This connector is compatible with the Raspberry Pi expansion header.

Back to top

Image Sensor Interface (J17)

The Image Sensor Interface (ISI) connects a CMOS-type image sensor to the processor and provides image capture in various formats. The SAM9X60-EK board contains an ISI connector that supports a 12-bit external camera. J17 is a 30-pin (2x15), 2.54-mm pitch header. It gives access to ISI I/O signals.

ISI and LCD interfaces are mutually exclusive and should be used one at a time.

Back to top

Red-Green-Blue (RGB) LED (LD1)

The SAM9X60-EK board features one RGB LED (LD1). It can be controlled by the user via GPIO, PWM I/O pins.

Back to top

Pushbuttons (SW1-SW4)

The SAM9X60-EK baseboard contains four pushbuttons:

  • USER_BTN (SW1): User push button which is available for user’s usage.
  • WAKE_UP (SW2): Wake Up will wake up the processor when it has been shut down by software.
  • nRST (SW3): Reset push button, when pressed the system resets.
  • DIS_BOOT(SW4): If kept pressed during power-up, the processor is prevented from booting off the on-board memories (QSPI and NAND Flash), thereby booting from other sources or into ROM code.

Back to top

LCD Interface (J15)

LCD Interface connector

The SAM9X60-EK contains a 24-bit LCD Interface, that supports a variety of LCD Displays. The Liquid Crystal Display Controller (LCDC) I/O lines are available on the baseboard 50-pin Flexible Flat Cable (FFC) / Flexible Printed Circuit (FPC) connector J15. The LCD connector J15 is on the bottom of the SAM9X60-EK board.

Display such as AC320005-5, which is a High-performance WVGA Display Module with maXTouch® technology can be connected.

A 50-pin FFC/FPC cable is included with the SAM9X60-EK kit.

ISI and LCD interfaces are mutually exclusive and should be used one at a time.

Back to top

Expansion

mikroBUS™ (J14)

mikroBUS™ socket is a proprietary communication and plugin standard for small interface boards called Click boards™ that extends the capabilities of the development board by offering Serial Peripheral Interface (SPI), UART, TWI, and PWM based sensors and devices. They are made by MikroElektronika, a producer and retailer of hardware and software tools for developing embedded systems.

Expansion options

Back to top

Power Options

The SAM9X60-EK can be powered by one of two methods:

  • J1: An external power jack to supply +5 VDC via a 2.1 mm center-positive plug
  • J7: Powered through the USB Micro-B connector USB port A

Power Options

USB-A (J7) is the default serial port used to communicate with the SAM-BA Monitor resident on the MPU.

Back to top

Jumper Summary

The Default Jumper Positions figure lists all the jumpers of the SAM9X60-EK and their default positions.

Jumper location

Default Jumper Positions

Back to top

What's Next?

After you have familiarized yourself with the features of the SAM9X60-EK, you may wish to learn more about:

Back to top