SAMA7D65 Curiosity Board - Quick Start Guide for MPLAB® Harmony v3

Last modified by Microchip on 2026/01/09 08:13

Introduction

Thank you for taking the time to evaluate the SAMA7D65 Curiosity development board. These instructions will guide you through running the demonstration application that comes with the kit. For a deeper dive into the features and capability of the kit, refer to the links provided in the "Learn More" section of this guide.

Pre-Requisites:

  • Confirm the following components are present in the box:
    • SAMA7D65 Curiosity board (P/N: EV63J76A)
    • SD card
    • USB Type-A to USB Type-C® cable (power)
  • Prepare the following hardware:
    • Windows® PC with an SD card reader and admin rights
    • Serial to USB dongle (FTDI)
    • Ethernet cable
  • Install the following applications on the Windows PC:

This quick start guide demonstrates how to perform an iPerf networking test between a Windows PC (acting as iPerf TCP Client) and the SAMA7D65 Curiosity board (acting as iPerf TCP Server).

Two network configurations are possible. Select the preferred one based on your local configuration:

  • Network configuration one:
    • The board and PC are connected directly with an Ethernet cable. In this case, a static IP will have to be manually assigned to the PC (admin rights needed).
  • Network configuration two:
    • The board and PC are connected through the local network infrastructure or a router. In this case, a Dynamic Host Configuration Protocol (DHCP) server will automatically assign an IP address to the board and the PC. (Ensure there are no IT restrictions for plugging the board on the local network.)
Information

Note: The "Troubleshooting" section at the bottom of this page for some more help.

MPLAB® Harmony v3 Demo Setup

Download the iperf.zip from the repository, GitHub-EV63J76A.

Back to Top


Unzip the downloaded iperf.zip file into any directory of your choice. Note the location where the files are unzipped. You will execute the iperf.exe from this location using a command prompt to run the TCP Client.

Back to Top


Download the harmony.img file from the repository, GitHub-EV63J76A.

Back to Top


Copy the downloaded file into the SD memory card using balenaEtcher.

Insert the SD memory card into the PC.

Download, install, and run balenaEtcher.

Select the downloaded harmony.img file.

balenaEtcher window Flash from File button

Click Select target to download.

balenaEtcher window Select Target button

Select the mounted SD card.

balenaEtcher  Select target window

Select Flash.

balenaEtcher window Flash button

The SD card will be ready for use once flashing is completed.

Back to Top


Connect the components as described in the following steps:

Ethernet cable to J14 connector

Other side of the Ethernet cable shall be plugged in the PC (network configuration one) or in a wall plug/router (network configuration two)

SD card inserted in the SD Boot J10 slot (bottom side of the board)

Serial to USB dongle to UART DEBUG J35 header on one side and to the PC on the other side

USB Type-A to USB Type-C cable to J3 USB Type-C port for power

board connection editor

Back to Top

Set Up the SAMA7D65 Curiosity Board Serial Terminal and Start the iPerf TCP Server

Set up the SAMA7D65 serial terminal on the PC.

On the PC, open a serial terminal with the following settings:

  • Baud Rate: 115200
  • Data: 8-bit
  • Parity: None
  • Stop: 1-bit
  • Flow Control: None

Open PuTTY.
putty icon

Open Windows Device Manager to find out which COM port to use; plug and un-plug the Serial-USB dongle and check which COMxx port appears and disappears (COM10 will be used in this example).

Open PuTTY > Category > Connection > Serial and configure the parameters as shown in the accompanying image. (Adapt the COM port to your local setup.)

Putty serial

Return to PuTTY > Category > Session and choose Serial for Connection type, then press Open.

Putty session

Back to Top


Press the RESET (SW4) button on the SAMA7D65 Curiosity board to force a reset.

When the system is ready, the SAMA7D65 serial terminal will show a prompt. This is the TCP server running on the Curiosity board and displayed on the PC.

In network configuration one, the board defines its own hardcoded IP address, 192.168.100.11. In network configuration two, the DHCP server will automatically assign an IP address to the board.

Verify that the iPerf MPLAB Harmony v3 application is running and displaying on the SAMA7D65 serial terminal.
TCP server Terminal

Press the Enter key to show the prompt.
TCP Server Terminal

Note the assigned IP address as it will be used to run the iPerf test. 

In this example, corresponding to network configuration one, the IP address is 192.168.100.11. In the case of network configuration two, the IP address will depend on your local environment.

Back to Top


Start the TCP Server on the SAMA7D65 Curiosity board by running the following command:

iperf -s -i 1

The SAMA7D65 serial terminal will show that the iPerf application is started and listening: 

TCP Server terminal

Back to Top

Configure the Windows PC and Start the iPerf TCP Client

In network configuration one, the PC ethernet IP address and mask must be manually configured (admin rights needed).

Open Windows network settings (the exact steps depend on your Windows version), and switch to manual configuration for the Ethernet interface.

Since the board IP is 192.168.100.11, manually configure, for example, the PC to IP as 192.168.100.2 and mask as 255.255.255.0.

IP address setup

In network configuration two, there's no need to manually set the PC IP address. The DHCP server will automatically assign one.

Back to Top


On the PC, navigate to the folder where iPerf was downloaded in Step 1 and open a command prompt.

Command prompt

Back to Top


Start the TCP Client iPerf in the command prompt by running the following command:

Information

Note: The IP address used must match the IP address recorded in Step 7.3.

.\iperf.exe -c 192.168.100.11 -p 5001 -i 1 -t 5

This will test the performance of the network transfers between the PC and the SAMA7D65 Curiosity board.

The TCP Client terminal will show the results of the test: 

iPerf2 Results

Back to Top


Return to the SAMA7D65 serial terminal and confirm the test results:

iPerf2 Server Results

 

Back to Top


Congratulations! Your SAMA7D65 board running MPLAB Harmony v3 is now connected over Ethernet to your PC.

What's next? See the "Learn More" section for more resources.

Back to Top

Troubleshooting

The SAMA7D65 serial terminal is not showing anything.

There are multiple possible reasons why the terminal does not show anything:

  • Double-check that the RX-TX signals of the serial cable are properly connected to the RX-TX signals of the board.
  • Double-check that the ground signal is properly connected.
  • Verify that the SD card contains the right files.

Running the iperf command on the PC terminal results in a "Connection refused" error.

[  1] tcp connect to 10.14.63.70 port 5001 failed (Connection refused) on 2024-05-31 11:43:21 (US Mountain Standard Time)

Verify that the IP address used when sending the iperf command matches the target IP address.
The terminal shows a RomBOOT message.
  • Verify that the SD card contains the right files.
  • Verify that the SD card is inserted properly.
IT restrictions forbid the plugging of SD cards in the PC. balenaEtcher can't be used. 

Another option for programming the SD card is to use the Microchip SAM-BA® In-system Programmer tool.

  1. Download and install SAM-BA ISP (v3.9 at least).
  2. Plug the USB Type-A to USB Type-C cable from the PC to J3 USB Type-C port for power and SAM-BA ISP connection.
  3. Plug the SD card in the SAMA7D65 board (not in the PC) and use the following SAM-BA ISP command to program the SD card:
    .\sam-ba.exe -p serial -b sama7d65-curiosity -a sdmmc -c write:harmony.img

Back to Top

Learn More

Back to Top