SAMA7G54 Curiosity Pro - Configure and Build at91bootstrap for Application Debugging with the MPLAB VS Code Extension

Last modified by Microchip on 2026/11/18 11:14

Purpose

The purpose of this tutorial is to

  • To understand the role of at91bootstrap in the system boot sequence
  • To configure at91bootstrap for debug support, enabling application loading via a debugger
  • To gain experience in customizing bootloader settings such as memory initialization, clock setup, and boot source selection
  • To build and generate a bootable binary image compatible with the target hardware

Overview

This tutorial focuses on configuring and building the at91bootstrap bootloader for a Microchip ARM-based platform. at91bootstrap acts as the second-stage bootloader responsible for initializing essential hardware components and preparing the system to load and execute the main application.

In this tutorial, participants modify at91bootstrap configuration to support both debugging and execution of bare-metal or MPLAB Harmony 3 applications flow

Configure at91bootstrap to debug a harmony application

The first step is to launch VS Code.

Ensure kconfig for MPLAB extension v1.5.0 or higher is installed by following the steps below:

  • Open VS Code and navigate to the Extensions view (Ctrl + Shift + X)
  • Search for “Kconfig for MPLAB” (Microchip official extension)
  • Check the installed version:
    • Ensure it is v1.5.0 or later
  • If not installed:
    • Click Install to add the extension
    • Restart VS Code after install/update (recommended)

Step1.png

If the popup shown below appears in VS Code while using Kconfig(or throughout at91bootsrap build and debug), press Esc to dismiss it. This will be fixed in the next version of the MPLAB UI plugin.Project Config- Missing compiler pop up

Clone at91bootstrap or download at91bootstrap from the github

Launch VS Code (File > Open Folder…) and select the at91bootstrap directory.

Step--2.png

Wait for the import to be completed. Verify the MPLAB project loads in the VS Code Explorer and at91boostrap.mplab.json file gets created. Then proceed to the next step.

Step--3.png

There are a number of default settings file for different hardware configuration that are intended to give you a starting point when configuring at91bootstrap. 

Examples of differences in the configurations are:

  • Boot media: SD/MMC vs QSPI (driver + where it looks for the next image)
  • Early hardware init: DDR timing/init, clocks, pinmux
  • Console/UART selection (where you see logs)
  • Debug behaviour: whether it stops/waits so a debugger can attach vs immediately loading the next stage

The Harmony app debugging flow expects a bootstrap that:

  • Initializes the board (especially DDR, clocks), and
  • Loads/starts your application image in the right place or jumps to your application DDR start address

sama7g54_curiosity_pro_bkptnone_defconfig (found under the configs folder in the at91bootstrap directory) is recommended for the SAMA7G54 Curiosity Pro debug flow used in these tutorials.

If sama7g54_curiosity_pro_bkptnone_defconfig not avalable under at91bootstrap configs directory, then dowload it from here and copy it to the at91bootstrap configs directory.

To load an existing at91bootstrap configuration in VS Code, first open the Command Palette by selecting View → Command Palette or pressing Ctrl + Shift + P, then type and select MPLAB Kconfig Configure to launch the Kconfig View for the project.

Once the Kconfig interface opens, verify that the at91bootstrap project is selected, and then click the Load button at the top of the Kconfig window. In the file selection dialog, navigate to the at91bootstrap/configs directory, select sama7g54_curiosity_pro_bkptnone_defconfig , and click Open.Load defconfig

The various boot configurations can be seen as depicted in the below

Boot Configuration options

Now click Apply.

Click Yes on the pop-up so the selected configuration is correctly saved to the .config file in the at91bootstrap directory.
This completes the configuration of at91bootstrap for debugging an MPLAB Harmony applicationSave Configuration

To build at91bootstrap follow the below steps:

  • Open Command Palette (Ctrl + Shift + P) from View → Command Palette and select Tasks: Run Task.
  • Choose the required task (e.g., clean - at91bootstrap (default)) from the list.
  • Then select Continue without scanning task output 
  • The task executes and shows clean output in the terminal

Step--8-1.png

 

  • Open Command Palette (Ctrl + Shift + P) from View → Command Palette and select Tasks: Run Task.
  • Choose the required task (e.g., build - at91bootstrap (default)) from the list.
  • Then select Continue without scanning task output 
  • The task executes and shows build output in the terminal

Step8-1.png

 

If build fails because python3.exe does not exist in PATH, while only python.exe is available, then do the following:

  • Using windows command prompt, navigates to the Python installation folder and creates a hard link using:

                                 mklink /H python3.exe python.exe

  • This creates python3.exe as an alias of python.exe.

Python 3 Error

If your build fails with an error like:

'rm' is not recognized as an internal or external command, operable program or batch file.

Change default terminal In VS Code, press Ctrl+Shift+P → select Terminal: Select Default Profile → choose Git Bash

Now when VS Code runs make, it will use Bash instead of PowerShell.

Step--9-1.png

The generated at91bootstrap.elf file under build/binaries/ can be used to debug an MPLAB Harmony application.

at91bootstrap

Back to Top

Results

At the end of this tutorial, participants successfully

  • Successfully configured at91bootstrap for:
    • Debug-based application loading
  • Generated the at91bootstrap binary image with required configuration
  • Verified proper initialization of system components during boot