Ensemble Graphics Toolkit: First Application Using Eclipse IDE™
Please see the Microchip Graphics Suite for the latest tools!
Introduction
Using the Eclipse IDE™ and Buildroot with the Ensemble Graphics Toolkit (EGT) helps simplify the compilation, remote execution and debugging of EGT applications.
In this training, you will download and install the Eclipse IDE for C/C++ Developers, configure and build a basic graphics interface for the SAM9X60-EK Evaluation Kit. You will run the application remotely and configure the Eclipse IDE for debugging.
A typical development flow path looks as follows:
- Download and configure the Buildroot build system. Download the Ensemble Graphics Toolkit source code. Build an SD Memory Card image (covered in the "Ensemble Graphics Toolkit: Preparing the Host PC and Target" page).
- Once the Buildroot build has finished, the output directory will contain the SD Memory Card image to boot Linux with the Ensemble Graphics Toolkit libraries. The build output also contains the cross toolchain for graphical development on the Host PC (covered in the "Ensemble Graphics Toolkit: Preparing the Host PC and Target" page).
- Download and configure the Eclipse IDE for compilation, remote execution and debugging (covered in this page).
By the end of this training, you will be able to develop simple graphical interfaces for the SAM9X60-EK using the Ensemble Graphics Toolkit.
Prerequisites
You have prepared the Host PC with all the development software tools and Ensemble Graphics Toolkit source code as explained in the topic, "Ensemble Graphics Toolkit: Preparing the Host PC and Target."
Procedure
Install the Eclipse IDE for C/C++ Developers
In this section, you will download, install, and configure the Eclipse IDE for C/C++ Developers. You will also download and install OpenJDK, the open-source implementation of the Java Platform, Standard Edition, as either OpenJDK or Java SE is required to run the Eclipse IDE.
Extract the archive file in the /opt directory:
$ sudo tar -zxvf eclipse-cpp-YYYY-MM-R-linux-gtk-x86_64.tar.gz -C /opt
Where YYYY-MM are the year and the month of the latest stable release.
Optional
On some Linux distributions, you may need to run this command:
$ sudo chown -R root:root /opt/eclipse
With Eclipse installed in the /opt directory, it can be accessed by any user.
Install OpenJDK-8:
$ sudo apt-get install openjdk-8-jdk
Create an Application Menu Shortcut for Eclipse
In this section, you will create an applications menu shortcut to launch the Eclipse IDE.
Change the directory to your home directory:
$ cd ~
With your favorite text editor, create a text file named eclipse.desktop.
Copy the following to the text file:
[Desktop Entry]
Name=Eclipse
Type=Application
Exec=/opt/eclipse/eclipse
Terminal=false
Icon=eclipse
Comment=Integrated Development Environment
NoDisplay=false
Categories=Development;IDE;
Name[en]=Eclipse
Save the text file.
Set the text file eclipse.desktop to be executable:
$ sudo chmod +x eclipse.desktop
Install eclipse.desktop:
$ sudo desktop-file-install eclipse.desktop
Create a symbolic link in /usr/local/bin:
$ sudo ln -s /opt/eclipse/eclipse /usr/local/bin/eclipse
Add the Eclipse IDE icon to be displayed with the shortcut:
$ sudo cp /opt/eclipse/icon.xpm /usr/share/pixmaps/eclipse.xpm
Start Eclipse and Create a Project
In this section, you will start the Eclipse IDE and create an Ensemble Graphics Toolkit project.
Start the Eclipse IDE:
Eclipse with ask you to select a directory for your workspace. Accept the default directory and click on the Launch button.

Eclipse will launch the workspace and display the welcome screen.

Create a Project
Start the process of creating a project by clicking on File > New > Project.
The New Project wizard will be displayed:
Select C/C++ Project. Click on the Next button.
The Templates for New C/C++ Projects will be displayed:

Select C++ Managed Build. Click on the Next button.
The C++ Project window will be displayed:

Enter a Project name of EgtProject. Under Project type, select Empty Project. Under Toolchains, select Cross GCC. Click on the Next button.
The Select Configurations window will be displayed:

By default, the Debug and Release configurations are selected. Click on the Next button.
The Cross GCC Command window will be displayed:

Enter the following information:
Cross compiler prefix: arm-buildroot-linux-gnueabi-
Cross compiler path: /home/<user>/buildroot-at91/output/host/bin
Click on the Finish button.

Adding a Source File
In this section, you will add a C++ source file to EgtProject.
To add a new C++ source code file, hover over EgtProject, right-click and select New > Source File.
A New Source File window will open.

Enter basic.cpp in the Source file box. Click on the Finish button.
The Eclipse IDE workspace now has the basic.cpp source file added to the project.

Enter the following source code to the basic.cpp window pane:
#include <egt/ui>
#include <iostream>
using namespace std;
using namespace egt;
int main(int argc, const char ** argv)
{
Application app;
TopWindow window;
Button button(window, "Press Me");
center(button);
window.show();
return app.run();
}
Save your program by selecting File > Save.
Configure Dependencies with the pkg-configure Tool
In this section, you will use the pkg-config tool located in the buildroot-at91 build to automate finding and configuring the correct dependencies to the Eclipse IDE to build your applications to run on the target.
On the Host PC, using your favorite text editor, add the following to your /.bashrc file:
export PKG_CONFIG_PATH =/home/<user>/buildroot-at91/output/host/arm-buildroot-linux-gnueabi/sysroot/usr/lib/pkgconfig/
Setting Build Properties
In this section, you will set the build properties for the EgtProject in the Eclipse IDE.
To set build properties, hover over EgtProject, right-click and select Properties from the menu at the bottom.
A Properties for EgtProject window will open:

In the left-hand pane of the Properties window select C/C++ Build > Tool Chain Editor.
Observe that the Current toolchain: dropdown box has Cross GCC selected.
Next, select C/C++ Build > Settings.
On the Tool Settings tab, select Cross Settings, and observe the following fields contain the following:
Prefix: arm-buildroot-linux-gnueabi-
Path: /home/<user>/buildroot-at91/output/host/bin

On the Tool Settings tab, select Cross G++ Compiler > Miscellaneous. Change the Other flags text box to the following:
-c -fmessage-length=0 `pkg-config libegt --cflags`

On the Tool Settings tab, select Cross G++ Linker > Libraries. To the right of the Libraries pane, click on the Add… (a little green plus next to a file icon). Add the following library: pthread
On the Tool Settings tab, select Cross G++ Linker > Miscellaneous. Enter the following into the Linker flags text box:
`pkg-config libegt --libs`

Click on the Apply and Close button. This will apply all the changes you have entered.
Building the Project
In this section, you will build the EgtProject.
To build the project, hover over EgtProject, right-click and select Build Project from the menu. Or you can click on the Build icon.
The Console window (bottom pane) will display the build progress.
At the completion of a successful build, a Debug folder in the Project Explorer window in the left pane. Note the files in the folder: makefile, sources.mk, objects.mk and subdir.mk.

You have successfully built EgtProject.
Run Application on Target Remotely
In this section, you will configure the Eclipse IDE to be able to run an application remotely on the target (SAM9X60-EK).
To set run properties, hover over EgtProject, right-click and select Run As > Run Configurations… from the menu.
In the left-hand pane, double-click on C/C++ Remote Application.

To setup a SSH connection with the target, click on the Connection New button.
A Create a new connection window will appear:

Select SSH from the dropdown box. Click on the OK button.
A New Connection window will appear:

Enter the following settings:
Connection name: Remote Host
Host: 10.0.0.20
User: root
Select Password based authentication
Password: <root_password>
Click on the Finish button.
In the Run Configurations window, enter the following in the Remote Absolute File Path for C/C++ Application: text box:
/root/basic
This is the location the basic.cpp executable will be loaded and run.
Click on the Run button.
Observe the WVGA Display on the target:
The basic.cpp executable is running remotely on the target.

To stop the program, press the Stop button (upper left hand, just below the menu bar).
The following information boxes contain information on the Application, TopWindow/Window, and Button classes used in the basic.cpp program.
Configure for Debugging
In this section, you will configure the Eclipse IDE to debug the EgtProject.
To configure the Debug Configuration, hover over EgtProject, right-click and select Debug As > Debug Configurations… from the menu.
The Debug Configurations window will appear:

In the left pane, select EgtProject Debug.
From the Main tab, observe the settings that you entered in the previous section:
Connection: Remote Host
Remote Absolute File Path for C/C++ Applications: /root/basic
Select the Debugger tab.

Enter the path to the arm-based debugger:
GDB debugger: /home/<user>/buildroot-at91/output/host/bin/arm-linux-gdb
Create a GDB initialization script by creating a text file named gdbinit in your home directory: /home/<user>. Enter the following text:
handle SIGILL nostop
set sysroot /home/<user>/buildroot-at91/output/host/arm-buildroot-linux-gnueabi/sysroot
Save the GDB initialization script.
On the Debug Configurations window, under the Debugger tab, enter the path to the GDB initialization script to:
GDB command file: /home/<user>/gdbinit
Click on the Apply button. Click on Close to close the Debug Configurations window.
Debugging
You can now click on the Debug As… icon (it looks like an insect, at the top in the ribbon) and select Local C/C++ Application.
Eclipse will change to the Debug Perspective and the application will halt at main(). Press Resume (F8) to continue execution and the application should appear on the WVGA display.
You can now use Eclipse to debug the application viewing variables, disassembling the code and enhancing debug experience.
Summary
In this training, you downloaded and installed the Eclipse IDE for C/C++ Developers. You configured and built a basic graphical interface for the SAM9X60-EK. You learned how to run and debug the application remotely from the Eclipse IDE.