Working with Multiple Layers and HW Overlays
Introduction
This section provides information on how to use Microchip Graphics Suite (MGS) Harmony Composer to take advantage of HW-accelerated compositing features of the integrated display controllers in Microchip's graphics-enabled MCUs and MPUs.
These features enable users to design complex GUIs and UI functions while minimizing the processing load on the main CPU.
Display Controllers and HW Overlays
Microchip's graphics-enabled MCUs and MPUs have integrated display controllers that process image data and send it to the display. This involves converting the digital representation of an image into signals that can be understood by the screen, such as timing signals for horizontal and vertical synchronization, and the actual pixel data.
These display controllers can have multiple HW overlays that allow an application or device to offload the rendering of certain content to dedicated hardware rather than processing it through the main CPU or even the GPU. The overlay unit is a separate hardware block that can handle tasks such as scaling, color conversion, and blending of the video or graphical content.
Below is an example of layers in the PIC32MZ DA GLCD display controller.

UI Layers and Compositing
Layers in User Interface (UI) design refer to the different levels at which elements are placed on the screen. Each layer can contain multiple components that are visually stacked on top of one another, much like layers of paper on a desk. This concept is crucial for organizing content, creating depth, and managing the complexity of interactions within the interface.
One common type of layer is the Background Layer which contains the background color, patterns, or images that form the foundation of the design.
Above the Background Layer can be Layer 1, which includes elements like headers, footers, navigation bars, and sidebars that provide the framework for the UI and help users navigate the interface.
Then on top can be Layer 2, which holds the primary information and elements that users interact with, such as text, images, buttons, and form fields.
These layers are then combined through a process called Compositing to create a final, cohesive image or interface that the user interacts with. This process is akin to how layers are managed in graphic design and photo editing software, where different elements can be stacked, organized, and manipulated independently before being merged into a single visual output.

Layer compositing is a fundamental concept in modern UI frameworks and design tools. It allows designers and developers to create complex, visually rich interfaces that are modular and easy to update.
HW Compositing
In Microchip's graphics-enabled MCUs and MPUs, compositing is performed using the HW overlays of the integrated display controllers. The MGL renders these layers in dedicated Frame Buffers in RAM which are read and combined by the Display Controller into a single output frame.

Using the HW overlays to composite these frames enables dynamic UI content with minimal load on the main CPU or GPU.
Multi-Layer UI Design using Microchip Graphics Suite (MGS) Harmony Composer
MGS Harmony Composer enables users to create multi-layer UI designs. The MGL works with the display controller drivers so these layers are rendered into their respective frame buffers that are then composited into a single frame.

To create a multi-layer design in MGS Harmony Composer, the following steps are performed:
- In the Screen Tree, click the + button to add a new layer.
- Add widgets to the new layer by dragging them from the Tool Box. A background panel widget was added for each layer. The background panel provides the library with a color to use for filling or clearing the background during a frame draw.
- Add a ClearScheme that will be used as a background scheme for layers with transparent backgrounds.
- This ClearScheme must be configured to have a Base color set to 0.
- The ClearScheme is used on the background panel for the upper layers with transparent backgrounds. This allows the lower layers to be visible in the composited frame.
- For the upper layers, the background panel Enabled property is unchecked. This ensures that touch input can propagate to the lower layers.
For more information on MGS Harmony Composer, refer to the "Microchip Graphics Suite (MGS) Harmony Composer User Guide".
Here's a visualization of how the layers in the above design are rendered to their respective frame buffers.

Configuring HW Overlays
HW Overlays are configured separately using the display controller driver. In MPLAB® Code Configurator (MCC) Harmony, the display controller component will have options to enable and configure each HW overlay.
By default, Composer Layer 0 is rendered to the frame buffer used by the base HW layer in the display controller. Composer Layer 1 is rendered to Overlay 1 frame buffer, and so on.
To ensure proper functionality, make sure that the correct HW overlays are enabled and configured to support the corresponding Layers in MGS Harmony Composer.
Here's an example Layer Configuration for the LCDC display controller for the Microchip graphics-enabled SAM9x60 MPU.

General Recommendations and Best Practices
Here are some examples of UI designs that can benefit multiple layers and best practices to maximize those benefits:
Use Multi-layers to Overlay Dynamic Content
Use multiple layers to separate dynamic content from static backgrounds, especially for UI designs with full-screen image backgrounds. By having the dynamic content in a separate layer, the background image does not need to be decoded and redrawn when the dynamic content changes.

Use Layers to Separate Dynamic Content and Overlay UI Controls
Another use of multiple layers is to overlay UI controls to the top layer and isolate it from the content layer. This has a couple of benefits:
- It ensures that the UI controls immediately get the touch input events, and
- The dynamic content can be rendered in a different format and does not cause redraw on other UI elements.
An example is a video player application where the bottom layer is used to show video frames in RGB565 format (for smaller size), and the video player controls are on the top layer.

Use Layers for Transparency Effects
HW overlays can be used to create transparent or semi-transparent effects on layers. Since the integrated display controller is used to alpha-blend these layers, the load on the CPU is minimal.

Advanced Techniques - Graphics Canvas
The Graphics Canvas is a middleware within MGS that makes it easy for users to leverage the HW features of the integrated display controllers in Microchip's graphics-enabled MCUs and MPUs. This can be used to perform complex GUI effects like sliding, fading, screen pre-rendering and animations without loading the CPU.
The Graphics Canvas middleware provides abstracted, user-friendly APIs to configure the display controller functions for these GUI effects.
Refer to "Using the Graphics Canvas" guide for more information.