Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Complex Breakpoint Latched-And
Last modified by Microchip on 2023/12/20 21:16
In addition to breakpoint sequences, a Latched-And (hardware AND) is available to AND a list of breakpoints. ANDed breakpoints can be useful when a variable is modified in more than one location and you need to break only when that variable is modified in one particular location.
Create a Breakpoint Latch-And
Right-click on an existing breakpoint or press Shift and click to select a group of existing breakpoints and right-click on the group.
From the pop-up menu, go to Complex Breakpoint and select Add a New Latched-And.
Enter a name for your Latched-And in the dialog box and click OK.
The breakpoint(s) will appear under the new Latched-And.
Add Existing Breakpoints to a Latch-And
Right-click on an existing breakpoint or press Shift and click to select a group of existing breakpoints and right-click on the group.
From the pop-up menu, go to Complex Breakpoint and select Move to Name, where Name is the name of the Latched-And.
Add a New Breakpoint to a Latch-And
Right-click on the Latched-And and select New Breakpoint.
Remove Breakpoints from a Latch-And
Right-click on an existing breakpoint or press Shift and click to select a group of existing breakpoints and right-click on the group.
From the pop-up menu, go to Complex Breakpoint and select Remove from Name, where Name is the name of the Latched-And.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.