Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Emulation Header Setup for MPLAB® X IDE
Last modified by Microchip on 2023/12/20 20:11
Set up MPLAB® X IDE to use an emulation header. Emulation header functionality is supported on MPLAB X IDE, but not on MPLAB IDE v8. Please use debug headers if you are still using MPLAB IDE v8.
Begin creating a project for a device supported by your emulation header using the Projects wizard (File > New Project). See MPLAB X IDE documentation for more on Projects.
Create a Project: Specify Header Product Number
In one step of the wizard you will have an opportunity to specify the emulation header product number (AC######).
Create a Project: Specify Debug Tool
In another step you will specify the hardware (debug) tool to which your emulation header is attached.
Develop Project Code
Once the wizard is complete, write code for your project.
Debug Your Code
Select Debug > Debug Project to run and debug your code.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.