Installing MPLAB® XC8 C Compiler
Download MPLAB® XC8 Installer
MPLAB® XC8 Compiler for your operating system. The compiler downloads are about halfway down the page.
Download the installer appropriate to your operating system.
Run Installer for Windows
Go to the location where you downloaded the installer. Unzip the downloaded file and run the installer:
xc8-vX.XX-windows-installer.exe
Depending on your Windows security settings, you may get a window asking if you are sure you want to run this program.
Answer Yes.
Run Installer for Linux
You may need to make the file executable. In a terminal, go to the directory where you downloaded the installer and run the command:chmod u+x
xc8-vX.XX-linux-installer.run
Then as root or using sudo, run the installer:
Run Installer for Mac
Go to the location where you downloaded the installer. Double-click on the downloaded file to unpack it and run the installer:
xc8-vX.XX-osx.app
You may get a warning message window. You can click on Open to continue.
Your computer's login and password need to be entered if you have enabled that protection for new installations. If you don't have a password enabled you can just click on OK to continue.
Setup
Click Next >
Click image to enlarge.
Accept License Agreement
Click on the radio button next to I accept the agreement.
Click Next >
Click image to enlarge.
Choose Installer
If you are installing the compiler for use on your machine only, click on the radio button next to Install compiler.
If you have a network license and are installing on a server, click on the radio button next to Install the Network License Server.
Click Next >
Click image to enlarge.
Installation Type
If you selected a network license server, provide the name of the network license server.
Click Next >
Click image to enlarge.
Installation Directory
Use the default installation location or choose a different one, if you prefer.
Click Next >
Click image to enlarge.
Compiler Settings
- Apply settings to all users of this machine
- Leave checked or uncheck if required in your environment.
- Add xc8 to the PATH environment variable
- Not generally required unless you plan to use XC8 from the command line (terminal or script).
Click Next >
Click image to enlarge.
Ready to Install Compiler
Click Next >
Click image to enlarge.
Setup
Wait while the installer unpacks and installs all the files.
Click image to enlarge.
Licensing Information
Click Next > if you:
- Have activated a license on a previous version of MPLAB XC8.
- Wish to use the free version of the compiler (some optimization features disabled).
Otherwise, choose to:
- Purchase a license (to receive an activation key that will unlock the Standard or Pro optimization features).
- Use the Pro evaluation version (reverts to the free version after 60 days).
- Provide an activation key.
Click Next >
Click image to enlarge.
Installation Complete
Click Finish
Click image to enlarge.