Buck Power Supply GUI Environment
Last modified by Microchip on 2024/06/24 06:32
The figure shown is an example of MPLAB® X Integrated Development Environment (IDE) with the MCP19110/11/18/19 Buck Power Supply Graphical User Interface (GUI) Plugin installed (bottom left) and the MCP1911X project opened (top left) in the Projects window. On the right are the Editor pane and Output window.
The MCP19110/11/18/19 – Buck Power Supply GUI Plugin is preset to be used with the MCP19111 Evaluation Board (ADM00397).