Digital Compensator Design Tool: Getting Started
Digital Compensator Design Tool Installation
The following steps describe how to install the Digital Compensator Design Tool (DCDT) Plugin.
If MPLAB® X IDE is already installed, go to Step 2. If not, download MPLAB X IDE.
Tools > Plugins: click on the Available Plugins tab, select Digital Compensator Design Tool Plugin, and click Install.
Accept the DCDT Plugin license agreements and then click Install.
After installation has completed, click Finish to restart MPLAB X IDE.
Launch DCDT
Select Tools > Embedded > Digital Compensator Design Tool.

The DCDT Chooser window appears. You can either open an existing project or create a new one.
Create New Project
Select Tools > Embedded > Digital Compensator Design Tool. Click Create a new project and the DCDT project window appears. You can create a Single-Loop System, Peak Current Mode Control, import an existing project, or open an example project.
Import Existing Project
This option copies all the settings from a previously created DCDT project into a new folder and allows you to give a new name to the project.