Module 1: Understanding the Shift from MPLAB® X IDE to VS Code®

Last modified by Microchip on 2026/10/12 11:09

Overview

In this lesson, we will establish the mental model you need to be successful with using the MPLAB® for VS Code®. You will learn how the VS Code–based firmware development workflow differs fundamentally from the traditional MPLAB X IDE, including how functionality is distributed across extensions and tasks. You will explore the VS Code interface and MPLAB Extensions components to orient yourself and reduce initial confusion when familiar MPLAB X IDE concepts appear in new forms.

Learning Objectives

Understand the new mental model for firmware development tasks using MPLAB for VS Code:

  • What has changed: Integrated Development Environment (IDE) vs. editor‑centric workflows
  • How MPLAB X IDE functionality is distributed across MPLAB for VS Code
  • Comparison table: MPLAB X IDE actions vs. VS Code workflows

Activity

Follow this guided walkthrough of the VS Code interface and MPLAB for VS Code components.

From MPLAB X IDE to VS Code: Expanding How You Work

MPLAB X IDE represents a traditional, integrated approach to embedded development. Most actions—creating projects, configuring tools, building and debugging—are performed through menus, icons and dialog boxes. This Graphical User Interface (GUI)‑driven model is familiar, highly discoverable, and continues to serve many developers well by clearly separating writing code from operating the tool.

MPLAB for VS Code introduces an alternative workflow—one that emphasizes flexibility and developer choice. Instead of relying primarily on menus and toolbars, actions can be invoked through commands, keyboard shortcuts, tasks, or the Command Palette. Project configuration lives in plain‑text files alongside source code, making settings explicit, visible and easy to version‑control. Importantly, this does not remove the ability to use graphical interfaces—it simply adds more ways to interact, allowing developers to choose what best fits their habits.

For many users, this results in a more fluid experience: coding, building, debugging, committing to Git, or reviewing issues can happen without leaving the editor or needing to reach for the mouse—though the option is always there. MPLAB X IDE is not being forcibly replaced; rather, VS Code offers an open, modular alternative to the monolithic IDE model. Developers can move at their own pace, adopt new workflows incrementally, and choose the environment that best supports how they work today—while gaining access to a broader ecosystem for tomorrow.

Mental Map Comparison

 MPLAB X IDEMPLAB for VS Code
Interaction ModelGUI‑driven with menus, icons and modal dialogsCommand‑driven using the Command Palette, tasks and shortcuts
Workspace ConceptApache Netbeans®‑based workspace, largely hidden from the file systemProject folder *is* the workspace
ConfigurationDialog‑based, changes applied via OK/ApplyFile‑based (JSON), changes are immediately visible and saved
(can also be viewed as Settings GUI)
Project StructureLogical (virtual) folders that may not match disk layoutPhysical folders that directly reflect the file system
Customization & EcosystemLimited to MPLAB X IDE pluginsFull VS Code ecosystem (Git, issue tracking, CI, AI, extensions)
User Interaction StyleMouse‑heavy, click‑through workflowsKeyboard‑centric, flow‑oriented workflows (mouse optional)
Installation ModelSingle, monolithic IDE installerModular extensions installed as needed

Make the Switch to MPLAB for VS Code

Back to Top

Overview of Working With MPLAB for VS Code

Once you start working with MPLAB for VS Code, you may notice some similarities to the MPLAB X IDE default view. 

1Activity BarIn the interface's left sidebar, the Activity Bar (1) displays the project along with its source and other files in Explorer view.
2Primary Side BarThe Primary Side Bar (2) displays the contents of the currently selected Activity Bar view.
3Editor Groups

In the upper middle of the interface is the Editor (3). The content shown relates to a selected file in the project (pic32cmjh-blink-led-mplab-harmony-mplab.json.)

4Panel

In the lower middle of the interface, there is Panel (4) for additional views. In this case, the project name is output to the terminal on opening.

5Secondary Side Bar

On the right side of the interface, in the Secondary Side Bar (5), is the Chat view.

6Status Bar

Finally, on the bottom of the interface is a Status bar (6).

For more details on the layout of the interface, see the Visual Studio Code documentation, "User interface" page.

VS Code-Project Example - Annotated

Back to Top

Find MPLAB for VS Code Extensions

VS Code has a rich ecosystem of extensions that enable specialized workflows. MPLAB for VS Code extensions are just one group of extensions that you can use. Add other extensions from the Visual Studio Code Marketplace.

To view details about an individual extension, click on it in the Marketplace or in VS Code if installed. For more information about extensions, see the "Extension Docs" page.

MPLAB Extensions Installer

Back to Top