Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Workflow for MPLAB® Extensions for Microsoft® Visual Studio® Code (VS Code®)
Last modified by Microchip on 2024/11/18 14:04
Workflow for MPLAB X IDE Users Familiar with Microsoft Visual Studio Code (VS Code)
If you are unfamiliar with MPLAB X IDE, please view either the "Tutorial" or "Basic Development and Debug Flow" online chapters of the MPLAB X IDE User's Guide.
To create a new project:
Run the command MPLAB: Create New Project and follow the wizard
To import an MPLAB X IDE project:
Open the project folder (File > Open Folder) and then follow the import suggestion
To configure a project:
Run the command MPLAB: Edit Project Properties (UI) or
Run the command MPLAB: Edit Project Properties (JSON) or
Open the project file manually
To build a project:
Use the keyboard shortcut Ctrl/Cmd + Shift + B or
Run the command MPLAB CMake: Full Build or
Use the Hammer tool
To create a debug configuration for a new project:
Run Debug: Add Configuration and select MPLAB Debugger
To launch a debug session:
Use the keyboard shortcut F5 or
Select the configuration from the Run and Debug view
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.