SAM9X60 Curiosity Board MPLAB® Harmony v3 Bare-Metal Examples

Last modified by Microchip on 2026/10/19 16:55

NoTitle/LinkHardware Board/KitDescription
1SAM9X60 Configure First Stage BootloaderSAM9X60 Curiosity This document explains how to configure the first-stage bootloader to load at91bootstrap from user-configured NVMs and configure boot sequences
2Configure the Second Stage Bootloader for SAM9X60-Based MPUsSAM9X60 Curiosity This document explains how to configure at91bootstrap to load an application from any one of the user-preferred Non-Volatile Memories (NVMs) or to debug an application on MPLAB® X IDE
3Write Boot Configuration Packet and Flash at91bootstrap, RTOS/Bare-metal Applications to External NVM SAM9X60 Curiosity This guide will explain how to use SAM-BA® ISPP software to write boot configuration packet and flash at91bootstrap, RTOS/Bare-metal applications to external NVM for the SAM9X60
4Getting Started on Graphics ApplicationSAM9X60 Curiosity Step-by-step guide on how to get started developing a graphics application with the SAM9X60-Curiosity development board on MPLAB X IDE
5Getting Started With Embedded Wizard GUI Application Development With MPLAB X IDESAM9X60 Curiosity This training module will guide you through the process of integrating Embedded Wizard project-generated code and its platform package into a FreeRTOS®-based MPLAB X IDE project using the SAM9X60 Curiosity development board
6Consumer Graphics (Snake Game)SAM9X60 Curiosity Snake game application on SAM9X60-Curiosity development board using MPLAB X IDE
7SAM9X60 Curiosity Development Board - FeaturesSAM9X60-Curiosity Features of the SAM9X60 Curiosity Development Board (EV40E67A)
8SAM9X60 Curiosity Development Board - ComparisonSAM9X60 Curiosity Feature-by-feature comparison between the SAM9X60-Curiosity Development Board and the SAM9X60-EK Evaluation Kit
9SAM9X60 Curiosity Development Board - Booting Demo Linux ImageSAM9X60 Curiosity Step-by-step instructions for booting a demo Linux image from an SD card
10SAM9X60 CuriositySAM9X60 Curiosity Get started on Linux OS development on the SAM9X60 Curiosity development board
11SAM9X60-EK – Configure and Build at91bootstrap for an MPLAB Harmony v3 Project with MPLAB X IDESAM9X60 Curiosity Configure and build at91bootstrap for an MPLAB Harmony v3 project with MPLAB X IDE
12Migrating a MPLAB Harmony v3 Software Framework Application from the SAM9X60-EK to SAM9X60-Curiosity: rtt_periodic_timeoutSAM9X60 Curiosity Migrating an MPLAB Harmony v3 application from SAM9X60-EK to SAM9X60 Curiosity: rtt_periodic_timeout
13Getting Started With Graphics on SAM9X60 Curiosity Development BoardSAM9X60 Curiosity Step-by-step guide showing customers how to get started with an MPLAB Harmony v3-based graphics application on the SAM9X60-Curiosity development board
14SAM9X60-Curiosity – Getting Started with MPLAB Harmony v3 Development: CSP Application: rtt_periodic_timeoutSAM9X60 Curiosity Step-by-step guide showing how to get started with an MPLAB Harmony-based application on the SAM9X60-Curiosity development board and debug using MPLAB PICkit™ 5 in-circuit debugger/programmer 
15SAM9X60-Curiosity – Configure and Build at91bootstrap to Load a MPLAB Harmony v3 Application from NAND Flash MemorySAM9X60-Curiosity Step-by-step guide showing how to configure and build at91bootstrap to load an MPLAB Harmony v3 application from a NAND Flash memory
16SAM9X60-Curiosity – Writing MPLAB Harmony v3 Application and at91bootstrap to NAND Flash Memory using SAM-BA ISPPSAM9X60-Curiosity Step-by-step guide showing how to write an MPLAB Harmony v3 application and at91bootstrap to a NAND Flash memory using SAM-BA ISPP
17at91bootstrap: Create a Custom Board ConfigurationSAM9X60 SeriesCustomizing a default configuration of at91bootstrap and build at91bootstrap under Linux®
18at91bootstrap: Customizing a Default ConfigurationSAM9X60 SeriesCreate a custom board configuration (almost from scratch) for the at91bootstrap bootloader
19SAM-BA ISPPSAM9X60 seriesDescription of SAM-BA ISPP and command line interface
20eXecute-In-Place (XIP) with Serial Flash Memories on MPUs Using MPLAB Harmony V3 (AN5218)SAM9X60-EKApplication note describing how to execute an MPLAB Harmony application from an on-board Quad Serial Peripheral Interface (QSPI) Flash memory
21QSPI-XIP- ExampleSAM9X60-EKMPLAB Harmony v3 application executed from QSPI flash on the SAM9X60 Evaluation Kit
22SAM9X60-EK Evaluation Kit - Attaching the TM5000 WVGA DisplaySAM9X60-EKAttach the TM5000 WVGA display with SAM9X60-EK