SAM9X75 Curiosity LAN Kit - MPLAB® Harmony v3 Examples

Last modified by Microchip on 2026/09/28 10:30

NoTitle/LinkDescription
1SAM9X75 Curiosity Development Board - IntroductionIntroduction to the SAM9X75-Curiosity Development Board
2SAM9X75 Curiosity Development Board - FeaturesFeatures of the SAM9X75 Curiosity Development Board
3SAM9X75 Curiosity Development Board - Console Serial CommunicationsConsole Serial Communications of the SAM9X75 Curiosity Development Board
4SAM9X75 Curiosity – Getting Started with MPLAB® Harmony v3 Development: CSP Application: rtt_periodic_timeoutFeature-by-feature comparison between the SAM9X60-Curiosity Development Board and the SAM9X60-EK Evaluation Kit
5SAM9X75 Curiosity – Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from SD™ Memory CardConfigure and build at91bootstrap to load MPLAB Harmony application from NAND flash memory
6SAM9X75 Curiosity – Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from NAND Flash MemoryConfigure and build at91bootstrap to load MPLAB Harmony application from NAND flash memory
7SAM9X75 Curiosity – Writing an MPLAB® Harmony v3 Application and at91bootstrap to NAND Flash Memory Using SAM-BA® ISPWrite an MPLAB Harmony v3 application and at91bootstrap to a NAND Flash memory using SAM-BA ISP
8SAM9X75 Curiosity – Configure and Build at91bootstrap to debug Harmony/Bare-metal applicationConfigure and build at91bootstrap for an MPLAB Harmony v3 project with MPLAB X IDE
9Adding Support for a Custom MIPI® Display on a SAM9X7 Series MPU under Linux®Detailed procedure to integrate support for a custom MIPI display on Microchip SAM9X7 Series microprocessors running Linux
10SAM9X75 Curiosity – Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from NOR Flash (QSPI) MemoryConfigure and build at91bootstrap to load MPLAB Harmony application from NOR flash memory
11SAM9X75 Curiosity – Writing MPLAB Harmony v3 Application and at91bootstrap to NOR Flash (QSPI) Memory using SAM-BA® ISPWrite an MPLAB Harmony v3 application and at91bootstrap to a QSPI-NOR Flash memory using SAM-BA ISP
12SAM9X75 Curiosity – Copy MPLAB® Harmony v3 Application and at91bootstrap to SD Memory CardCopy two binary images, harmony.bin (an MPLAB Harmony v3 Software Framework application) and boot.bin (second-stage bootloader, at91bootstrap), to an SD memory card
13Power Monitoring (PAC1934) on SAM9X75 Curiosity Development Board Using MPLAB® Harmony ApplicationLearn how to measure power consumption on the SAM9X75 Curiosity Development Board using the PAC1934 power monitoring Integrated Circuit (IC)
14SAM9X75 Curiosity - IoT Thermostat Application Using Embedded Wizard GUI+ WINCS02+ RNBD+ MQTT Training with Hands-on LabsEight structured hands-on lab sections, designed to guide you step by step through the development of a complete IoT Thermostat application using the SAM9X75 Wireless Curiosity Kit
Lab 1 - How to Create an MPLAB X IDE ProjectDetailed steps on how to create an MPLAB X IDE project
Lab 2 - How to Integrate a Temperature Sensor to an MPLAB X IDE ProjectDetailed steps on how to integrate a temperature sensor to an MPLAB X IDE project
Lab 3 - How to Integrate the RNBD Module to MPLAB X IDE to Establish Bluetooth® CommunicationDetailed steps on how to integrate the Roving Networks Bluetooth Device (RNBD) module to MPLAB X IDE to establish Bluetooth communication
Lab 4 - How to Integrate the WIxCS02 M.2 Wi-Fi® Module Card to an MPLAB X IDE Project to Establish Wi-Fi CommunicationDetailed steps on how to integrate the WIxCS02 M.2 Wi-Fi module card to an MPLAB X IDE project to establish Wi-Fi communication
Lab 5 - How to Integrate MQTT to an MPLAB X IDE Project to Publish and Subscribe Data To/From a Cloud BrokerDetailed steps on how to integrate MQTT to an MPLAB X IDE project to publish and subscribe data to/from a cloud broker
Lab 6 - How to Integrate an Embedded Wizard GUI Project With an MPLAB X IDE ProjectDetailed steps on how to integrate an embedded wizard GUI project with an MPLAB X IDE project
Lab 7- Debugging and Testing the IoT MPLAB Harmony ApplicationDetailed steps on how to debug and test the IoT MPLAB Harmony application
Lab 8 - Running the Pre-built MPLAB Harmony IoT Application from the SD CardDetailed steps on how to run the pre-built MPLAB Harmony IoT application from the SD card
15SAM-BA In-System Programmer (ISP)Description of SAM-BA ISP and command line interface
16eXecute-In-Place (XIP) with Serial Flash Memories on MPUs Using MPLAB Harmony V3 (AN5218)Application note describing how to execute an MPLAB Harmony application from an on-board QSPI Flash memory
17SAM9X75 Curiosity Development Board: Fast Boot DemonstrationSAM9X75 fast Boot demonstration