Buck Power Supply Graphical User Interface (GUI) Operation
To launch the Buck Power Supply Graphical User Interface (GUI) from the drop-down menu, select Tools > Embedded > MCP1911X GUI Plugin.


Project Configuration
To display the project properties, right-click on the project name inside the Projects view and select Properties. While the provided project should already be correctly configured to ensure proper hardware and software configuration, please ensure that the correct hardware tool (PICkit™ 3 or ICD3) and C compiler (XC8) are highlighted in the Hardware Tool and Compiler Toolchain windows, respectively. This section describes a list of settings that must be checked before beginning to use the tools.
If multiple projects are opened on MPLAB® X Integrated Development Environment (IDE), the plug-in will work in the project selected as Main Project.
Set a Main Project
Two methods may be used:
Right-click on a project's top node and select Set as Main Project from the popup menu.

Right-click in a blank area of the project tree and select Set Main Project > Your Project Name.

Learn More
- Buck Power Supply Graphical User Interface
- Buck Power Supply GUI System Components
- Buck Power Supply Graphical User Interface (GUI) Requirements
- Buck Power Supply GUI Installation
- MCP19111 Digitally Enhanced Power Converter
- PICkit 3 Training
- MPLAB X IDE Training
- MPLAB X IDE Plugins
- MCP19110/11/18/19 - Buck Power Supply Graphical User Interface User's Guide