Memory Xplorer Evaluation Kit Setup
Microchip's Memory Xplorer supports multiple evaluation kits with more coming. This section describes how to assemble the kit, connect it to Memory Xplorer and configure Memory Xplorer for the selected device.
Assemble the evaluation kit
To start using the evaluation kit, plug the Socket Board into the USB Base Board using the 2x5 connectors. Refer to the appropriate evaluation kit user guide for details.
Add the serial EEPROM device
Once both boards are connected, install a Microchip EEPROM device into the Socket Board socket, making sure to note that the Pin 1 indicator on the PCB matches the Pin 1 indicator on the device.
The following figure illustrates an SOIC device properly seated in its respective socket and highlights the Pin 1 indicator on the PCB.
Device in SOIC socket:
Insert the evaluation board into the computer USB port
Memory Xplorer will confirm socket detection in the Event Log if the setup is correct.

A list of matching devices will be shown. There will be four columns of information:
- Protocol
- Device name
- Device memory size (in bits)
- An icon indicating which devices have extra features, e.g. Serial Number, EUI-48, etc. See the Terminology section in this lesson or product datasheet for more information.

Select your device
The Start button will turn green. If not, verify the device protocol selected in the Protocol filter matches the selected device. See the Troubleshooting section for more suggestions.

Click the Start button
Memory Xplorer will read the serial EEPROM, update the Editor Panel, and make additional functionality available. If successfully connected, the Event Log will show Memory Xplorer successfully connecting the USB and socket, current voltage, and read operation status.
Check the Troubleshooting section if you need help.

What's Next?
Now your evaluation kit is set up, you can learn about the various features of Memory Xplorer. A good starting point is the Editor Panel overview. Or if you are ready to program your serial EEPROM device, see the Memory Xplorer Write, Read and Erase Operations for details.
Learn More
- Memory Xplorer Embedded Memory Evaluation Platform
- Evaluation kits
- SPI Introduction
- I2C Bus Introduction
- What is the Single Wire Interface (SWI) protocol?
- Unique ID (UID)
- Media Access Control (MAC) addresses
- EEPROM Endurance Tutorial (AN1019)
- Sample Order Page
- Serial EEPROM page
- Microchip Purchasing and Client Services
- Intel Formatted HEX Files