Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Set Up Trace Hardware
Last modified by Microchip on 2023/12/20 19:58
To use trace, you will need the ribbon cable and emulator interface board that comes with the emulation header. Connect one end to the emulation header. Connect the other end to the emulator. For more information on complete hardware setup and connections, refer to Emulation Header Hardware Setup. For details on trace connectors, see Trace Hardware.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.